Subscribe to RSS

Tag Archives: SmartPort

TRELLEBORG TO TALK SMARTPORT, TURNKEY LNG SOLUTIONS AT GASTECH 2018

By Richard Hepworth, President of Trelleborg’s marine systems operation


Trelleborg will discuss SmartPort at Gastech in Barcelona (17-20 September), in addition to showcasing its range of game-changing LNG transfer technology. I am also delighted to reveal that as part of Gastech’s main conference program, my colleague Andrew Stafford, Technical Director at Trelleborg’s marine systems operation will present a technical paper discussing the latest in Ship-Shore Link (SSL) technology that has set the industry standard in large-scale LNG transfer for nearly 20 years. Vincent Lagarrigue, Director of Oil & Marine Hoses at Trelleborg’s oil and marine operation will also present a technical paper that outlines how cryogenic floating hose technology is unlocking new possibilities in small to medium-scale transfer and LNG bunkering.

On stand (K160), experts from Trelleborg’s marine systems operation will be on hand to discuss SmartPort, a technology platform that powers the critical interface between ship and port, on land and at sea. The SmartPort platform connects port operations, allowing operators to analyze asset performance and use data to improve decision making. The system integrates assets like fenders, mooring equipment, ship performance monitoring, and navigation systems through a network of sensors.

Trelleborg’s oil and marine operation will be highlighting how their Cryoline floating cryogenic hoses technology is transforming LNG transfer operations in both near-shore and offshore environments. Cryoline technology was specially developed to address pressing infrastructure challenges in the LNG market, enabling turnkey projects that drastically reduce the capex and environmental impact of LNG import infrastructure. It also opens up new locations to ship-to-shore and ship-to-ship transfer, even in challenging weather conditions, and increases safety and operability of FLNG loading and offloading by enabling transfer in tandem configuration.

Trelleborg is able to provide the most integrated and configurable solutions at every interface of the LNG transfer operation. However, realizing the critical interface between ship and port, on land and at sea, SmartPort provides a unique overview of the ‘vessel turnaround’ process, and data extraction points throughout it – both on board the vessel and in the port, and in the interface between the two. We look forward to exhibiting a number of solutions within our SmartPort portfolio including AutoMoor, a rope-free automated mooring system for smarter, safer and more efficient berthing operations; SafePilot, a new generation of piloting and navigation software; as well as our Integrated SSL and Emergency ShutDown System (ESDS) for both large and small-scale LNG transfer and fueling. We’ll also showcase our Quick Release Hooks (QRH) which enable mooring lines to be safely secured and quickly released; as well as its SmartDock Laser Docking Aid System for vessel approach and berthing operations.

In addition to the latest in SSL technology, Andrew’s session will highlight how close co-operation between all parties has enabled Q-LNG to develop their LNG bunkering project from the early adoption for the Harvey Gulf OSV fleet through to the latest requirements for fully flexible bunker vessels. The presentation will also discuss how process safety is improved and training is facilitated by using digital fiber optic link technology with redundancy to ensure compatibility with ESD systems, telephony and cargo process data from any LNG fuelled vessels.

Together, these technologies enable revolutionary new models and thinking for LNG transfer, unlocking new possibilities throughout the transfer zone. Vincent’s session will explore how this was demonstrated in September 2017, when technology from both operations was used in the first sea launch of the Universal Transfer System (UTS), a plug-and-play turnkey developed with Connect LNG. The success of this launch demonstrated the vast potential for new infrastructure possibilities that Trelleborg’s technology enables.

For more information, come and see us on stand K160 at Gastech.

 

COLLABORATION IS KEY – TRELLEBORG HOSTS THCC SEMINARS

By Richard Hepworth, President, Trelleborg marine systems operation

Vessel sizes are becoming larger, competition is increasing and broader alliances between shipping lines are being established. These factors combine to put increased pressure on ports and terminals. Our industry is famously conservative, but change is coming quickly. There will be a need for more collaboration – as different stakeholders have different strengths. This will make partnerships throughout the supply chain and across industries critical.

After signing a memorandum of understanding (MoU) in 2017, strategically, this is what both we and Third Harbor Consultants Company (THCC) are doing. Collaborating. To further innovation and enable improvements for our ports and vessels. Recently, this saw Trelleborg host two technical seminars (20 & 21 June) in China with consultants and engineers from THCC and CCCC Water Transportation Consultants Company (WTCC).

The seminars provided consultants and engineers from THCC and WTCC with a comprehensive overview of SmartPort by Trelleborg, which powers the critical interface between ship and port, on land and at sea. SmartPort connects port operations, allowing operators to analyze performance and use data to increase efficiencies, improve safety and improve ROI for ports and vessels alike. The system integrates assets like fenders, mooring equipment, ship performance monitoring, and navigation systems through a network of sensors.

The seminars also provided insight on two solutions that fall under the SmartPort portfolio. The first being AutoMoor, Trelleborg’s rope-free, automated mooring system that uses smart technologies to enable faster berthing and improve safety levels within the port environment.

The second was Smart Fender, a marine fender load monitoring system that can be used to measure both the impact on fenders when a vessel berths, and the ongoing force applied as the vessel continues to bear against them whilst docked. When analyzed, the data obtained has the potential to be used in several ways: such as developing a deeper understanding of berthing dynamics, which in turn could assist with future fender and wharf design, and further, feed into the revision of safe and acceptable berthing operations and procedures.

Additionally, load data may be used to determine when maintenance is needed, or indeed, a replacement fender is required. In the event of an accident, or a fender failing, the data can be used to provide information as to why – providing valuable data for insurance claims and helping ports and shipping lines to avoid the costly downtime associated with disputes.

For more on SmartPort by Trelleborg, visit: http://www.trelleborg.com/en/marine-systems/smartport

GOING GREEN!

By Richard Hepworth, President, Trelleborg’s marine systems operation

Sustainability is one of the key challenges facing the marine industry. Being able to implement environmentally-friendly business practices is not simply a tick box exercise, it is a commercial imperative. Organizations of all kinds within our diverse sector are looking to find new ways to improve the efficiency of operations to ensure assets are fully optimized and working in as sustainable a way as possible.

The Green Maritime Forum is an important event in the calendar as it brings together experts who are involved in researching and developing sustainable solutions and enables them to share their latest thinking and breakthroughs with industry stakeholders. Trelleborg is attending this year’s Hamburg-based event and the managing director of our Danish operations, Tommy Gulhammer-Mikkelsen will be giving a talk on the future of ports and piloting, looking in particular at how automation technologies are improving the interface between vessel and port to maximize operational efficiencies.

It is these technological advances that are the key drivers in developing more sustainable maritime solutions. Real-time data capture and analysis, such as that provided by SmartPort by Trelleborg, can significantly improve port and vessel throughput and turnaround which in turn has a positive impact on fuel efficiency. Similarly, we are currently developing an Adaptive Under Keel Clearance system (AKUC) for our customers which will provide real-time measurement and take into account constantly changing environmental factors to potentially enable ships to carry more cargo, save on dredging costs and increase safety.

More efficient operations should create more sustainable operations. Technology is the enabler that can better connect the various elements of the supply chain, establishing a connected eco-system based on common standards that allows traditional and new assets to communicate with each other easily and effectively.

If you are attending the Green Maritime Forum then I’d encourage you to go to Tommy’s session, or to find out more about Trelleborg’s sustainable solutions, visit the website.

NEW WHITEPAPER PROVIDES OVERVIEW OF BIG DATA IN THE MARITIME SECTOR

By Richard Hepworth, President of Trelleborg’s marine systems operation

Trelleborg’s marine systems operation has launched a new whitepaper bringing together the latest news and thinking on big data in the maritime sector, highlighting how and where these technologies are being implemented and the key application areas that will deliver future operational efficiencies for ports and terminals.

Titled ‘The use of Big Data in the maritime industry’, the whitepaper explores how the maritime industry can better understand the opportunities that big data offers, both now and in the longer term.

Big data has the potential to transform our industry. Through application and insights, big data is creating new opportunities to drive innovation and deliver tangible operational efficiencies across the shipping world.

But the collection of information alone is not enough. It is the analysis of this data and the actionable insights it provides that will transform and increase the efficiency of day-to-day operations across the shipping industry in years to come.

This is a time of huge change for our industry. The advancement of automation, and the exponential rise in data it brings, mean disruption on a scale that ‘shipping’ has never seen before. Those that invest now in the architecture that empowers collaboration between smart assets, will be best equipped to face the future.

SmartPort realises the critical interface between ship and port,
on land and at sea. This gives Trelleborg a unique overview of the ‘vessel turnaround’ process, and data extraction points throughout it – both on board the vessel and in the port, and in the interface between the two. Trelleborg is seeking to educate the marine industry about the importance and potential of this interface.

SmartPort is Trelleborg’s answer to the need for a standardized way to collect and store data. It’s a technology platform that connects port operations, allowing users to analyze asset performance and apply data insights, to improve day-to-day decision making for optimised operations; improved safety, reduced costs, greater sustainability and increased revenue return.

To read the whitepaper, visit: http://ow.ly/ClMF30ihvQc

 

TRELLEBORG TO LEAD ASTM INTERNATIONAL TASK GROUP FOR NEW LIQUIFIED GAS SSL STANDARD

By Richard Hepworth, President, Trelleborg’s marine systems operation

Linked ship-shore Emergency Shut-Down (ESD) systems have been a recognized safety feature of traditional LNG carrier transfer operations for many years. However, provisions of linked ESD systems in the emerging trades of LNG FSRU and LNG bunkering, as well as the non-methane gas distribution between ships and terminals, are being hampered by the lack of an accepted industry standard for equipment, to achieve the required connection.

To that end, I am delighted to reveal that Technical Director, Andrew Stafford has been appointed as Task Group Leader of the ASTM International Standard for Liquefied Gas Ship Shore Links’ (SSL) standardization group.

Andrew and the team that will be built for the Task Group will look to develop an industry-wide standard, covering the minimum requirements for the safe transfer of liquefied gasses using SSLs. Ultimately providing recommendations for how we can take welcome steps forward in evolving the inter-connection of ESD systems for universal adoption.

ASTM International is a globally recognized leader in the development and delivery of voluntary consensus standards. Today, over 12,000 ASTM International standards are used around the world to improve product quality, enhance health and safety, strengthen market access and trade, and build consumer confidence.

Trelleborg has supplied SSL systems since 1996 and is the leading supplier globally, having received contracts for over 650 systems. The company’s extensive knowledge and experience led to the development of Trelleborg’s SMART SSL system. This system can be supplied as a stand-alone one for existing tonnage or for integration with other key safety and monitoring systems. It provides a significant improvement over previous operator interfaces and simplifies control and set-up.

Trelleborg’s SSL falls within the company’s SmartPort portfolio. SmartPort is Trelleborg’s answer to the need for a standardized way to collect and store data. It is a technology platform that connects port operations, allowing users to analyze asset performance and apply data insights, to improve day-to-day decision making.

For more information about Trelleborg’s SMART SSL system, visit: http://ow.ly/QHC330foLgy

 

TRELLEBORG LAUNCHES AUTOMOOR FOR SMART, ROPE FREE MOORING

By Richard Hepworth, President, Trelleborg’s marine systems operation

Docking and mooring can play a critical role in increasing throughput of an individual berth and overall port facility. No matter the application, ports and terminals worldwide are under pressure to increase throughput. However, trying to do so at the same time as dealing with increasing vessel sizes can be difficult. Optimizing operational windows is an effective route to improving efficiency and one that AutoMoor enables by reducing the time taken to moor vessels.

AutoMoor is a rope-free, automated mooring system that uses smart technologies to enable a faster berthing process and improve safety levels within the port environment. Using vacuum technology to rapidly attach to and secure a vessel at berth, it reduces vessel motions, and continuously monitors all mooring loads acting on the vessel at berth, providing live data to the operator to optimize day-to-day port and terminal operations. It also minimizes personnel involvement to reduce human error and improve safety.

With mooring units that provide real time data to monitor vessel mooring loads, Trelleborg is offering the automated technology needed to compete effectively in today’s complex, global landscape.

Automated mooring technologies minimize downtime by reducing the effects passing ships have on moored vessels. When using mooring lines, operators may need to interrupt operations, costing time and money in delayed product transfer. Using an automated mooring system to dampen vessel motions and extend the range of conditions in which efficient transfer can take place can have huge implications for efficiency.

AutoMoor is also intended to help ports and terminals become more environmentally efficient, because vessels can be secured in under a minute and released in 30 seconds. This reduces vessel idling time and reduces the time tug boats are required alongside the vessel until the mooring operation is complete, cutting emissions overall.

Trelleborg’s AutoMoor solution falls under the operation’s SmartPort portfolio. SmartPort is Trelleborg’s answer to the need for a standardized way to collect and store data in marine applications. It’s a technology platform that connects port operations, allowing users to analyze asset performance and apply data insights, to improve day-to-day decision making.

The most important aspect of SmartPort is the open API structure which enables collaboration with third party systems and third party assets. Historically, Trelleborg has supplied many products for the port environment, from fenders to mooring equipment to ship performance monitoring to navigation and piloting systems: each of which can have their own sensors fitted. By adopting SmartPort architecture, all of these systems and more can be brought under one cloud based system.

To find out more about AutoMoor, download the brochure and discover the smarter approach to docking and mooring: http://ow.ly/ARF330fiAaa

 

LOOKING FORWARD TO THE ANNUAL PORT DEVELOPMENT MENA FORUM

By Richard Hepworth, President, Trelleborg’s marine systems operation

I’m pleased to announce that we are sponsoring the fourth Annual Port Development Middle East and North Africa (MENA) Forum at the end of September in Dubai, UAE.

The Forum discusses how the MENA region can keep up with disruptive new technologies to maintain its status as a maritime power.

I will also be presenting at the conference on the topic of digital and data-driven technologies and our SmartPort offering, as part of a session about successful port digitization, automation and security.

My presentation is entitled ‘A Smarter Approach to port infrastructure and communication’, and will discuss the need for greater collaboration between stakeholders, examine the changing role of equipment suppliers, discuss the storage, analysis and sharing of data through standardized, open systems and go on to explain how we are responding to these evolving market needs with SmartPort.

Other speakers include representatives from the Dubai Maritime City Authority, SOHAR Port and Freezone, Hamburg Port Authority and the General Authority for Suez Canal Economic Zone.

They will discuss the biggest challenges to the region and debate best-practice methodologies for securing, constructing and operating port infrastructure in the Middle East and North Africa. I’m very much looking forward to hearing what the other speakers have to say, and having some constructive conversations about the future of port development in our region.

The fourth Annual Port Development MENA Forum will take place from 26-28 September at the Dusit Thani Dubai.

 

TRELLEBORG FOCUSES ON OPTIMIZING PILOTING AND NAVIGATION IN US WORKSHOP

By Tommy Mikkelsen, Managing Director of Trelleborg’s marine systems operation in Denmark

Piloting requires the safest, most efficient and reliable technology. It demands exceptional performance, ease of operation and high position accuracy to facilitate optimum approach, berthing and departure. With that in mind, we hosted a technical seminar and workshop designed to help marine pilots keep up-to-date with Smart technology to ensure the efficiency and safety of navigation and piloting operations. The seminar and workshop was held 4 – 5 May at the Baltimore Marriott Waterfront Hotel in Baltimore, U.S.

The event saw myself discuss Trelleborg SmartPort, a technology platform that connects disparate port operations, providing holistic, real-time oversight which allows users to analyse the performance of assets and identify areas for optimization.

In addition, the President of the American Pilot Association, Captain Jorge Viso, also had his say on the evolution of piloting technology. Representatives from both the Association of Maryland Pilots and San Francisco Bar Pilots (SFBP) were also on hand to discuss Trelleborg SafePilot which uses state-of-the-art software and smart technology to help pilots and ports optimize safety and efficiency in their day-to-day operations.

SafePilot offers the latest in navigation & piloting and port systems. Developed in conjunction with working marine pilots from across the world, SafePilot offers the most up-to-date user-friendly PPU (Portable Pilot Unit) software available. Using touch screen technology to make it easy to operate, this intuitive PPU software consists of separate modules to meet different maritime operational needs, from docking and river through to lock.