Subscribe to RSS

Tag Archives: Pneumatic fender

RAISING THE BAR FOR PNEUMATIC FENDER MANUFACTURE

By Mishra Kumar, Technical Director for Marine Fenders at Trelleborg’s marine systems operation

Trelleborg’s marine systems operation has launched a new whitepaper highlighting the impact of the manufacturing process on the performance, safety, and longevity of pneumatic fenders.

Titled ‘Pneumatic Fenders: Manufacturing Methods Matter’, the whitepaper explores the difference in fenders manufactured using the airbag manufacturing method without employing a mold, and fenders manufactured conventionally using a mold, to highlight the impact of the manufacturing process on fender quality.

Pneumatic fenders are extensively used for ship-to-ship transfers mid sea, double banking operations, and as vessel-to-berth at dock/jetties. Therefore it is vital that they are not only of high quality, but are extremely reliable, to guarantee effective performance in even the harshest environmental conditions.

Each and every pneumatic fender must comply with the ISO 17357-1:2014 standard to ensure they follow the correct manufacturing process. The major concern for the industry is that there is an influx of manufacturers employing airbag production methods resulting in fenders that don’t usually comply with all of the recommended manufacturing process guidelines or compound properties as specified under the ISO 17357-1:2014 standard.

By using the conventional method, whereby the entire fender is built inside a mold and vulcanized with it in an autoclave, a clear positive impact is seen on the appearance, dimensional stability and the bonding between layers, leading to a more reliable and long lasting fender.

To read the whitepaper, visit: http://ow.ly/QYNt30itWOP

 

TRELLEBORG LAUNCHES NEW ISO17357-1:2014 COMPLIANT PNEUMATIC FENDER

By Richard Hepworth, President of Trelleborg’s marine systems operation

Remaining true to its principle of innovation, Trelleborg’s marine systems operation has launched a new ISO17357-1:2014 compliant, high performance pneumatic fender designed to address the evolving needs of ports, terminals and offshore ship-to-ship transfer applications.

The new quality assured fender features a thinner, lighter body for easier transportation and handling, improved netting and hemispherical ends designed to offer superior functional performance and enhanced continuity of end fittings for optimum deflection capability.

In addition to improvements in the design of the fender, materials have been engineered to ensure a stronger overall performance. After detailed research into optimum tire cord reinforcement, we have re-evaluated our materials to enhance fender performance.

Unlike other manufacturers that use synthetic tire cords for only the body of the fender and chafer fabric at both hemispherical ends, we now use 100% synthetic tire cord for the construction of the entire fender. This directly enhances the fender’s operational ability because synthetic tire-cord has a higher tensile strength than chafer fabric. By incorporating the synthetic tire cord into the entire fender, the stability, longevity, and shape retention of the fender are all significantly enhanced.

Demonstrating our best practice approach to delivering superior products that incorporate optimum, high quality materials, our new pneumatic fender goes above and beyond the minimum requirements of the ISO 17357-1:2014 standard which recommends the use of synthetic tire-cords but does not make it mandatory.

Trelleborg not only meets but exceeds the demands of the ISO17357-1:2014 standard with quality assurance documents and test results shared in a comprehensive, fully-authenticated supporting document package. Proof data, inner and outer rubber material specifications and pressure test data are all included as standard for even greater peace of mind.

Many suppliers however utilize low cost, low quality, non-compliant materials and fail to perform stringent materials and product testing to the requirements of the ISO standard. For instance, for the external rubber layer composition of a fender which plays a major role in its longevity, many suppliers use rubber compounds which fail to comply with the new ISO requirement.

In addition, a large number of suppliers also turn to low cost recycled rubber-based compounds. Others use chafer fabric, a cheaper alternative to tire-cord. The chafer fabric is unable to provide Minimum Endurable Pressure (MEP) at 0% and 60% deflection, which is imperative for pneumatic fenders to work efficiently in harsh conditions.

Many suppliers also reduce the number of plies, or use a reinforcing layer made from a low-cost suboptimal combination of chafer fabric and tire cord as they lack the basic design concepts to produce high quality pneumatic fenders.

Specifiers should also be wary of inefficient, cost-reducing methods used by suppliers such as the use of a heating jacket instead of a mold during the curing process. It is also critical that specifiers are aware of manufacturers claiming to be supplying ISO17357-1:2014 compliant pneumatic fenders which are actually produced using the ‘airbag’ construction method. Products constructed in this manner, are not compliant with ISO17537-1 and will not guarantee the level or longevity of performance of a ‘true’ pneumatic fender.

To find out more about the new ISO17357-1:2014 compliant, high performance pneumatic fender, download the Product Application Briefing now: http://ow.ly/tncb301PFOc.

TRELLEBORG TO SHOWCASE NAVIGATION BUOYS AT SEAWORK 2016 INTERNATIONAL

Trelleborg’s marine systems operation will showcase its innovative range of IALA compliant modular navigation buoys at Seawork 2016 International from the 14 to 16 June at Mayflower Park, Southampton, England.

Building on the strength of a long-standing foam elastomer and marine aluminium superstructure system, we boast a comprehensive range of polyethylene constructed navigation buoys, completing our portfolio of navigation and marker buoys to suit all environments.

With that in mind, Seawork provides the ideal platform to showcase our modular system, which provides an easily transported option to cut down turnaround time and enable fast installation, as they can be shipped in sections and assembled on site.

Manufactured from impact resistant, colour-fast, UV stable materials and comprising of sectional hull pieces filled with marine grade, water-resistant foam, Trelleborg’s range of IALA compliant modular navigation buoys are built around a hot dipped galvanised steel core. Available as standard in diameters ranging from 1.25 to 3.6 meters, Trelleborg will also manufacture precisely to specification where required.

We’ll also showcase our range of SeaGuard fenders which can be deployed floated or suspended, against a quay wall or for ship-to-ship operations. SeaGuard fenders suit all sites with small or large tidal changes. They also work just as well on new or old structures.

In addition, Trelleborg’s SeaGuard fenders combine a durable, non-marking finish with low maintenance. SeaGuard fenders will never sink or deflate. Even at the end of their first service life they can be returned to the factory for refurbishment before going back to work.

Trelleborg’s highly durable floating foam and pneumatic fenders are available for short-term or long-term rental. Readily available, they can be delivered and installed within days to any location across Europe and Asia Pacific.

As Europe’s largest commercial marine and workboat exhibition, Seawork International attracts over 7,500 industry professionals each year. Comprising an exhibition, conference and awards, Seawork International is regarded as the industry’s one-stop-shop, providing buyers, legislators and influencers with direct access to the commercial marine and workboat market, its products, its innovations and its people.

To find out more, visit Trelleborg at Seawork 2016 on booth number PY154.