Subscribe to RSS

Tag Archives: Oil

TRELLEBORG TO TALK SMARTPORT, TURNKEY LNG SOLUTIONS AT GASTECH 2018

By Richard Hepworth, President of Trelleborg’s marine systems operation


Trelleborg will discuss SmartPort at Gastech in Barcelona (17-20 September), in addition to showcasing its range of game-changing LNG transfer technology. I am also delighted to reveal that as part of Gastech’s main conference program, my colleague Andrew Stafford, Technical Director at Trelleborg’s marine systems operation will present a technical paper discussing the latest in Ship-Shore Link (SSL) technology that has set the industry standard in large-scale LNG transfer for nearly 20 years. Vincent Lagarrigue, Director of Oil & Marine Hoses at Trelleborg’s oil and marine operation will also present a technical paper that outlines how cryogenic floating hose technology is unlocking new possibilities in small to medium-scale transfer and LNG bunkering.

On stand (K160), experts from Trelleborg’s marine systems operation will be on hand to discuss SmartPort, a technology platform that powers the critical interface between ship and port, on land and at sea. The SmartPort platform connects port operations, allowing operators to analyze asset performance and use data to improve decision making. The system integrates assets like fenders, mooring equipment, ship performance monitoring, and navigation systems through a network of sensors.

Trelleborg’s oil and marine operation will be highlighting how their Cryoline floating cryogenic hoses technology is transforming LNG transfer operations in both near-shore and offshore environments. Cryoline technology was specially developed to address pressing infrastructure challenges in the LNG market, enabling turnkey projects that drastically reduce the capex and environmental impact of LNG import infrastructure. It also opens up new locations to ship-to-shore and ship-to-ship transfer, even in challenging weather conditions, and increases safety and operability of FLNG loading and offloading by enabling transfer in tandem configuration.

Trelleborg is able to provide the most integrated and configurable solutions at every interface of the LNG transfer operation. However, realizing the critical interface between ship and port, on land and at sea, SmartPort provides a unique overview of the ‘vessel turnaround’ process, and data extraction points throughout it – both on board the vessel and in the port, and in the interface between the two. We look forward to exhibiting a number of solutions within our SmartPort portfolio including AutoMoor, a rope-free automated mooring system for smarter, safer and more efficient berthing operations; SafePilot, a new generation of piloting and navigation software; as well as our Integrated SSL and Emergency ShutDown System (ESDS) for both large and small-scale LNG transfer and fueling. We’ll also showcase our Quick Release Hooks (QRH) which enable mooring lines to be safely secured and quickly released; as well as its SmartDock Laser Docking Aid System for vessel approach and berthing operations.

In addition to the latest in SSL technology, Andrew’s session will highlight how close co-operation between all parties has enabled Q-LNG to develop their LNG bunkering project from the early adoption for the Harvey Gulf OSV fleet through to the latest requirements for fully flexible bunker vessels. The presentation will also discuss how process safety is improved and training is facilitated by using digital fiber optic link technology with redundancy to ensure compatibility with ESD systems, telephony and cargo process data from any LNG fuelled vessels.

Together, these technologies enable revolutionary new models and thinking for LNG transfer, unlocking new possibilities throughout the transfer zone. Vincent’s session will explore how this was demonstrated in September 2017, when technology from both operations was used in the first sea launch of the Universal Transfer System (UTS), a plug-and-play turnkey developed with Connect LNG. The success of this launch demonstrated the vast potential for new infrastructure possibilities that Trelleborg’s technology enables.

For more information, come and see us on stand K160 at Gastech.

 

SEE YOU AT KORMARINE 2015!

By Richard Hepworth, President, Trelleborg’s marine systems operation

At the end of October, we will be exhibiting at Kormarine 2015, a leading marine trade exhibition which takes place at the BEXCO (Busan Exhibition & Convention Center), in Busan, Korea and covers international marine, shipbuilding, offshore and oil and gas industries.

At the event, we’re pleased to be demonstrating our new Integrated Ship Shore Link (SSL) and Emergency Shutdown System (ESDS) for the marine LNG industry.

Attracting around 40,000 visitors, Kormarine is the largest marine trade exhibition, covering both commercial and military shipbuilding.

Trelleborg Marine Systems has a major centrer in Busan supporting all of our Oil and Gas Transfer and Vessel Technology products. At the event, representatives from our Busan office, and from the wider business, will be on stand to meet attendees and discuss the latest developments in the Korean market, as well as our experiences in the LNG industry globally.

As well as the new integrated ESDS/SSL system we will also be showcasing our ship performance technology as well as our Worldwide Service capability.

To find out more, visit us at Kormarine 2015 on booth number 5K17, in Hall 5, from the 20 to 23 October. We look forward to meeting you there!

TRELLEBORG ENGINEER JOINS PRESTIGIOUS GASTECH YOUNG ENGINEER FOUNDATION

By Richard Hepworth, President of Trelleborg’s marine systems operation

We call ourselves the Performance People because we ensure the right support is in place for our customers from conceptual design to after sales care. To enable us to deliver truly end-to-end service to our customers, we’re committed to the professional development of our staff.

With that in mind, I am delighted to reveal that Matthew Walker, Project Engineer at our operation in Australia has been handpicked to join the esteemed Gastech Young Engineer Foundation (GYEF).

Given the growing need to attract young talent to the energy industry, the GYEF recognizes and supports the next generation of engineers. The GYEF’s committee, which represents several leading figures in the global energy industry, selected Matthew as one of just 80 successful candidates from several hundred applicants.

Bolstering the professional development of engineers in the early stages of their career, the GYEF has awarded Matthew access to an exclusive package of educational and networking opportunities. This includes a complementary delegate pass for the 2015 Gastech Conference & Exhibition in Singapore (27th – 30th October 2015), providing the opportunity to connect and network with peers and industry leaders. In addition, Matthew has also been awarded a lifetime membership to Gastech’s Young Engineer Alumni and granted unlimited access to online mentoring from thought leaders through a dedicated section of the GYEF website.

For Matthew to be recognized so enthusiastically at such an early stage in his career is a phenomenal feat. We hold a long-standing commitment to the professional development of our staff, and this is testament to our ability to produce industry ready talent.

To find out more about The Gastech Young Engineer Foundation, visit: http://www.youngengineersfoundation.com/

TRELLEBORG TAKES TO PREVENTION FIRST 2014 TO DISCUSS END-TO-END SERVICE OFFERING

October’s “Prevention First: An Onshore and Offshore Pollution Prevention Symposium & Technology Exhibition”, provided the ideal platform to discuss the importance of technical and aftersales support, and the service Trelleborg Marine Systems offers.

Here at Trelleborg, we offer a complete range of fendering, docking and mooring solutions, as well as a one-stop-shop for technical, operational and maintenance support.  Our most recent Barometer Report revealed a huge gap in the maintenance requirements of port owners and operators, and the support that suppliers are able to provide. So it was great to use the exhibition as a platform to connect with stakeholders to discuss where suppliers fall short and what more we can do to give them the support they need.

Ultimately, successful projects engage suppliers from the earliest possible stages, to get input and guidance on what will be the most appropriate solution on a case-by-case basis. That’s why we provide stakeholders with support from the earliest design stages to aftersales support. In particular, it was great to discuss our program for the North American market, and its development in accordance with OCIMF, SIGTTO and PIANC guidelines.

We also had a comprehensive team of sales and technical experts on stand to take visitors through the role Trelleborg played in the first phase of implementation of the Marine Oil Terminal Engineering and Maintenance Standards (MOTEMS). The standards apply to all existing and new marine oil terminals in California, and include criteria for inspection, structural analysis and design including mooring and berthing requirements.

The Prevention First exhibition is organised by the California State Lands Commission (CSLC), which sets the requirements for marine jetties throughout California.

The full results of Trelleborg’s latest Barometer Report, which details a wide range of findings from the industry survey, is available now as a free download from: http://www.trelleborg.com/en/Marine-Systems/Home/

 

 

 

TRELLEBORG BECOMES PIANC PLATINUM PARTNER

Here at Trelleborg, we have a longstanding association with PIANC. Not only do we have a number of people involved in technical working groups, but we’ve also participated in and sponsored a number of world congress events. After being the Platinum AGA sponsor of the 33rd PIANC World Congress at the beginning of June, I am delighted to reveal that we have cemented our commitment to best practice by becoming a PIANC Platinum Partner. As a manufacturer of mission critical port equipment, its essential to us to share knowledge with the industry body that guides standards across the board.

With PIANC continuing to set best practice guidance for so many, and varied, issues pertinent to waterborne transport infrastructure, they felt it was important to have a supplier on board that could contribute across such a broad spectrum.

With our expertise extending from shore-based infrastructure, to oil and gas and LNG; we’re well placed to contribute to a number of areas PIANC work within.

This year’s Congress resolution, set forth by PIANC, will investigate ongoing and emerging trends, technologies and business models. With that said, we here at Trelleborg look forward to being involved in contributing to this important discussion going forward.

For more information about PIANC, visit: www.PIANC.org

SEE YOU AT GASTECH 2014

My colleagues and I will be attending Gastech 2014 in Korea next week. As one of the world’s favorite meeting places for energy professionals working in the oil and gas industry, Gastech provides the ideal platform for us to exhibit our latest product innovations and get some deeper insights into what other delegates see as the most critical issues in the market.

At the show, we’ll be showcasing our brand new Compact Series of Quick Release Hooks (QRHs) which have been designed specifically for smaller and simpler mooring applications, where traditional large and more complex QRHs are not appropriate.

The hooks combine the knowledge of our vastly experienced engineering team with FEA software, and provide an optimized solution for less complex and lower rating mooring applications. They represent a viable alternative to bollards for commercial ports and fuel wharfs, and could also be used in the rapidly developing small-scale LNG sector.

In addition, we’ll also have our Seatechnik™ Universal Safety Link (USL) on stand, a truly innovative product optimized for the small scale LNG sector. The USL was developed in response to the market requirement for a Ship-Shore Link (SSL) which addressed the needs of the LNG marine fuel and small scale transfer market.

We have also developed a new LNG application briefing, ‘Leading-edge Performance in LNG”, which we’ll have available for delegates to take away from our stand. It discusses the evolution of docking and mooring solutions, fender systems and transfer technology across a range of LNG applications.

If you’re heading to Gastech 2014, which will take place at the Kintex, Korea from the 24th to the 27th March, make sure you come and see us on stand F160.