Subscribe to RSS

Tag Archives: Navigation Buoy

TRELLEBORG TO SHOWCASE NAVIGATION BUOYS AT SEAWORK 2016 INTERNATIONAL

Trelleborg’s marine systems operation will showcase its innovative range of IALA compliant modular navigation buoys at Seawork 2016 International from the 14 to 16 June at Mayflower Park, Southampton, England.

Building on the strength of a long-standing foam elastomer and marine aluminium superstructure system, we boast a comprehensive range of polyethylene constructed navigation buoys, completing our portfolio of navigation and marker buoys to suit all environments.

With that in mind, Seawork provides the ideal platform to showcase our modular system, which provides an easily transported option to cut down turnaround time and enable fast installation, as they can be shipped in sections and assembled on site.

Manufactured from impact resistant, colour-fast, UV stable materials and comprising of sectional hull pieces filled with marine grade, water-resistant foam, Trelleborg’s range of IALA compliant modular navigation buoys are built around a hot dipped galvanised steel core. Available as standard in diameters ranging from 1.25 to 3.6 meters, Trelleborg will also manufacture precisely to specification where required.

We’ll also showcase our range of SeaGuard fenders which can be deployed floated or suspended, against a quay wall or for ship-to-ship operations. SeaGuard fenders suit all sites with small or large tidal changes. They also work just as well on new or old structures.

In addition, Trelleborg’s SeaGuard fenders combine a durable, non-marking finish with low maintenance. SeaGuard fenders will never sink or deflate. Even at the end of their first service life they can be returned to the factory for refurbishment before going back to work.

Trelleborg’s highly durable floating foam and pneumatic fenders are available for short-term or long-term rental. Readily available, they can be delivered and installed within days to any location across Europe and Asia Pacific.

As Europe’s largest commercial marine and workboat exhibition, Seawork International attracts over 7,500 industry professionals each year. Comprising an exhibition, conference and awards, Seawork International is regarded as the industry’s one-stop-shop, providing buyers, legislators and influencers with direct access to the commercial marine and workboat market, its products, its innovations and its people.

To find out more, visit Trelleborg at Seawork 2016 on booth number PY154.

TRELLEBORG TO SHOWCASE NAVIGATION BUOYS AT SEAWORK 2015 INTERNATIONAL

Ashley Tasker, Global Business Development Manager for Marine Products at Trelleborg Marine Systems

I am delighted to reveal that we will showcase our innovative range of IALA compliant modular navigation buoys at Seawork 2015 International, the largest and fastest growing international commercial marine and workboat exhibition and conference held in a European working port environment (16th to 18th June).

Our unique, comprehensive range of navigation buoys provides a solution to fit all demanding requirements – in addition to our standard range, we are able to manufacture to specification where required. The modular system provides an easily transported option to cut down turnaround time and enable fast installation, as they can be shipped in sections and assembled on site.

Manufactured from impact resistant, colour-fast, UV stable materials and comprising of sectional hull pieces filled with marine grade, water-resistant foam, Trelleborg’s range of IALA compliant modular navigation buoys is built around a hot dipped galvanised steel core. Available as standard in diameters ranging from 1.25 to 3.6 meters, Trelleborg will also manufacture precisely to specification where required.

We will also be taking the opportunity to showcase our range of Foam / Elastomer constructed mooring buoys. Thanks to their low maintenance, self-fendering resilient foam bodies and their ease of handling and repair whilst offshore, these are rapidly replacing traditional steel mooring buoys.

Our booth will also feature our pneumatic and foam fenders. As an ideal ship protection medium for load sensitive structures such as LNG vessels and ocean platforms, our range of pneumatic fenders feature high energy absorption with low reaction force. While our foam fenders are super tough due to a unique manufacturing process and have high energy absorption for their reactive load.

If you’re heading to Seawork 2015 and want to find out more, come and see us at booth number A187.

Alternatively, visit: http://www.trelleborg.com/en/Marine-Systems/