Subscribe to RSS

Tag Archives: LNG

TRELLEBORG TO ATTEND 6TH ANNUAL LNG BUNKERING SUMMIT

By Richard Hepworth, President of Trelleborg’s marine systems operation

Trelleborg’s marine systems operation will showcase its Universal Safety Link (USL) technology at the 6th annual LNG Bunkering Summit (29 -31 January) in Amsterdam.

The LNG Bunkering Summit brings together global players from leading ports, LNG terminal operators, ship operators, ship owners, LNG suppliers, and LNG technology providers to develop strategic partnerships and common strategy to drive the LNG Bunkering market forward. The three-day event will provide attendees with perspectives across the entire supply chain on decision making, planning, development, operation, safety and training processes that have allowed them to successfully move forward in the LNG Bunkering market.

With more LNG capacity coming on stream year on year we are seeing increasing demand not just for large scale transportation of cargoes but also for more FSRU applications and of course the growth of LNG bunkering and fueling for marine vessels. All of these applications have in common one key requirement. The safe, efficient and timely transfer of LNG from one tank system to another. One key critical element in achieving this is the ship-shore interface.

Paul Radage, Sales Director at Trelleborg’s marine systems operation UK, will take to the stage to discuss the importance of ship-shore link systems and the requirement  to ensure that newly installed systems remain compatible not only with each other but also with the existing installed base.

The safe, efficient transportation and transfer of LNG as a cargo has had an enviable safety record over its 40 year history. We have all, at some point, had a part to play in delivering that record and during the LNG Bunkering Summit we will learn from each other about how we will seek to maintain this record while rising to the new challenges and applications the industry presents.

For more information about The LNG Bunkering Summit or to register your attendance, visit: https://lngbunkering.iqpc.co.uk/

 

 

TRELLEBORG SUPPLIES SUITE OF SOLUTIONS TO FIRST FLOATING LNG SHIP-TO-SHORE SYSTEM

By Richard Hepworth, President of Trelleborg’s marine systems operation

The recent successful test of the Universal Transfer System (UTS) conducted with Connect LNG and Gas Natural Fenosa is tangible evidence of the new applications that Trelleborg’s suite of products for jettyless LNG transfer can unlock in this challenging field.

The UTS transferred LNG from the Skangas-chartered LNG carrier Coral Energy to the onshore terminal at the Norwegian port of Herøya on October 7 and is now in full commercial operation. A ‘plug and play’ solution, the UTS requires no modifications to the LNG carrier – instead, the platform maneuvers offshore to meet a vessel, removing the need for costly and environmentally intensive dedicated small/medium-scale LNG vessel harbor and jetty structures.

The system consists of Trelleborg’s Cryoline LNG hoses, attached to a floating platform, which incorporates Trelleborg’s ship-shore link technology and a selection of our marine fender systems.

The UTS shows that LNG infrastructure doesn’t need to be bound by the same thinking that underpins transfer solutions for fossil-based energy. Instead, it demonstrates how new ideas are creating the foundations for safe, efficient and convenient infrastructure that can keep pace with the rapid evolution of the LNG market, both as a power source and marine fuel.

The UTS is an important forward thinking development. Our Universal Safety Link (USL) and the Sea Guard and Super Cone fenders are used in many LNG applications already. Integrating them into such an innovative solution as this will help ensure the safe, efficient transfer of LNG into markets and locations that would have previously been considered uneconomic. We are proud to be part of a project that promotes the expansion of the LNG value chain.

The UTS increases the operability of an LNG terminal, as the hose and platform can be retracted when not needed, or when harsh weather conditions would present hazards. The platform-based solution can either function as a standalone unit, or enhance a larger terminal’s ability to handle deliveries to and from a broader range of vessels. Trelleborg service engineers were present during the first commercial LNG transfer of 400m3, and will support further commissioning operations.

A range of Trelleborg technologies make this new model of LNG transfer possible. Cryoline is the first floating hose of its kind to receive the coveted EN1474-2 accreditation, using flexible rubber-bonded hose technology to minimize boil-off and withstand fatigue harsh environmental conditions. Extra safety is provided by an integrated monitoring system using fiber-optic technology.

We also supplied our industry-leading USL 8810 to monitor the LNG transfer process. A triple fiber optic, five pin SIGTTO and pneumatic system was supplied to ensure all round flexibility for the platform for any visiting vessel Our Sea Guard fenders were specified for use at the front of the UTS to absorb berthing impact against the larger LNG vessel prior to attachment to the vessel. While to reduce the impact of the tug vessels on the UTS, our Super Cone (SCN) fenders enable the tugs to safely push the UTS from shore into position for transfer operations.

I’ll leave you with a few comments from Magnus Eikens, Chief Commercial Officer of Connect LNG and José Miguel Moreno, Director at Gas Natural Fenosa:

Magnus commented: “Trelleborg’s expertise in fluid handling and LNG transfer has made it an invaluable partner in this project. The Cryoline LNG hose is an integral part of this solution, thanks to its durability, flexibility, and safety features. What’s more, its ship-shore link technology and marine fender expertise is vital in supporting UTS LNG transfer operations.”

“The innovation demonstrated by Trelleborg and Connect LNG has delivered a game-changing solution for the LNG industry. We now have a market-ready system that opens a world of possibilities in the LNG small and medium scale business thanks to this collaboration,” added Jose.

 

 

 

 

 

TRELLEBORG TO OPEN 2017 LNG SHIP-SHORE INTERFACE CONFERENCE

By Richard Hepworth, President of Trelleborg’s marine systems operation

Trelleborg’s marine systems operation will deliver the welcoming address at The LNG World Shipping Ship/Shore Interface Conference, which will be held at the ILEC Conference Centre (stand 1) in London, England, 16-17 November 2017.

Organized by LNG World Shipping, The LNG Ship/Shore Interface Conference provides invaluable best practice insight to all stakeholders in the LNG transportation supply chain. This event will focus on the ship/shore interface, where LNG carrier and terminal operations link to load or discharge LNG and the most delicate point in the supply chain for cargo and custody transfer systems, berthing and escort tugs, mooring and jetty arrangements and cargo-handling equipment performance.

Delivered by Dave Pendleton, Managing Director of Trelleborg’s marine systems operation UK, the welcoming address will discuss the importance of innovation and collaboration around the ship shore interface for LNG transfer.  At the conference, Trelleborg will also provide an update on the latest developments in the mid-scale LNG market. Andrew Stafford, Technical Director of Trelleborg Marine Systems operation in UK will present how Trelleborg’s latest SmartPort enabled Gen 3 ship shore link has been designed to provide complete flexibility for increasing variety of LNG markets and applications. ’.

At 258MT last year was a record for LNG trade, and with more liquefaction and import capacity coming on line in the near future and over 800MT of proposed liquefaction projects in planning, innovation around the ship-shore interface will be a key enabler in supporting the growth, flexibility and diversification of the LNG market.

From terminals to trucks, jetties to jettyless, floating to fixed, ship to shore, ship to ship industry professionals from many different disciplines will share their views about how the ship shore interface may evolve to the benefit of our customers.

The safe, efficient transportation and transfer of LNG as a cargo has had an enviable safety record over its 40 year history. Over that period many different ideas have been brought forward which are now accepted industry practice and industry standards. The LNG Ship/Shore Interface Conference will provide the ideal platform to discuss our commitment to maintaining this record by helping ports, terminals and vessels take a smarter approach to interfaces between units in LNG transfer, which can have a huge impact on overall efficiency.

For more information about The LNG Ship/Shore Interface Conference or to register your attendance, visit: http://www.lngshippingconference.com

TRELLEBORG TO EXHIBIT AT 8TH MOTORSHIP GAS FUELLED SHIPS CONFERENCE

By Richard Hepworth, President of Trelleborg’s marine systems operation

Trelleborg’s marine systems operation will showcase its Universal Safety Link (USL) technology at The 8th Motorship Gas Fuelled Ships Conference (13 – 15 November) onboard the Viking Mariella in Helsinki.

The conference offers a technical perspective on the innovation and investment driving the uptake of LNG, methanol and other low-flashpoint fuels in the commercial shipping sector. With a focus on knowledge sharing from a variety of projects, the conference examines the latest advances in vessel design and operation, propulsion, supply infrastructure and associated technology.

At the conference, Steve Ward, Technical Sales Manager of Trelleborg’s marine systems operation UK, will also take to the stage to provide an overview of the developments in Emergency Shutdown (ESD) and Ship-Shore Link (SSL) System technology over the last decade. He will discuss the need for standardisation and compatibility across markets.

The conference provides the ideal platform for us to connect with ship owners and operators, LNG carriers, shipbuilders, as well as port and terminal owners and operators in the region to discuss the importance of specifying compatible and proven technology and its role in ensuring the safe, efficient transportation and transfer of LNG as a fuel.

For more information about The Motorship Gas Fuelled Ships Conference, visit: http://www.motorship.com/gfsconference

 

 

TRELLEBORG TO LEAD ASTM INTERNATIONAL TASK GROUP FOR NEW LIQUIFIED GAS SSL STANDARD

By Richard Hepworth, President, Trelleborg’s marine systems operation

Linked ship-shore Emergency Shut-Down (ESD) systems have been a recognized safety feature of traditional LNG carrier transfer operations for many years. However, provisions of linked ESD systems in the emerging trades of LNG FSRU and LNG bunkering, as well as the non-methane gas distribution between ships and terminals, are being hampered by the lack of an accepted industry standard for equipment, to achieve the required connection.

To that end, I am delighted to reveal that Technical Director, Andrew Stafford has been appointed as Task Group Leader of the ASTM International Standard for Liquefied Gas Ship Shore Links’ (SSL) standardization group.

Andrew and the team that will be built for the Task Group will look to develop an industry-wide standard, covering the minimum requirements for the safe transfer of liquefied gasses using SSLs. Ultimately providing recommendations for how we can take welcome steps forward in evolving the inter-connection of ESD systems for universal adoption.

ASTM International is a globally recognized leader in the development and delivery of voluntary consensus standards. Today, over 12,000 ASTM International standards are used around the world to improve product quality, enhance health and safety, strengthen market access and trade, and build consumer confidence.

Trelleborg has supplied SSL systems since 1996 and is the leading supplier globally, having received contracts for over 650 systems. The company’s extensive knowledge and experience led to the development of Trelleborg’s SMART SSL system. This system can be supplied as a stand-alone one for existing tonnage or for integration with other key safety and monitoring systems. It provides a significant improvement over previous operator interfaces and simplifies control and set-up.

Trelleborg’s SSL falls within the company’s SmartPort portfolio. SmartPort is Trelleborg’s answer to the need for a standardized way to collect and store data. It is a technology platform that connects port operations, allowing users to analyze asset performance and apply data insights, to improve day-to-day decision making.

For more information about Trelleborg’s SMART SSL system, visit: http://ow.ly/QHC330foLgy

 

TRELLEBORG TO SHOWCASE SMARTER APPROACH TO LNG AT SSM 2016

Trelleborg’s marine systems operation will showcase its SeaTechnikTM Universal Safety Link (USL) and the Integrated Ship-Shore Link (SSL) and Emergency Shut-Down system (ESDS) for the LNG industry at SMM 2016 International. The event will be held from 6 to 9 September at Hamburg Messe, Hamburg, Germany.

The USL 8810 is specifically designed to support the growing LNG marine fuel and small scale LNG market, while the innovative design of the Integrated SSL and ESDS provide significant installation cost reduction for ship builders. Both the Integrated SSL and ESDS also provide improved operator feedback and maintenance diagnostics for owners of large scale LNG carriers. Trelleborg has also designed an ESDS system to support the USL 8810 for small scale operations.

LNG operations require the safe, efficient and timely transfer of LNG from one tank to another. Trelleborg currently has SSL systems on 450 LNG carriers, 25 FSRUs, 100 LNG terminals and over 30 USL systems in the growing LNG marine fuel and small scale market. All supported by a global service team on a 24/7 basis.

With an unrivalled track record spanning decades of service to the port and harbor, marine, offshore and shipbuilding industries, Trelleborg is a world leader in the design and manufacture of advanced Marine Fenders, Oil & Gas Transfer systems, Docking & Mooring systems, as well as Navigation & Piloting solutions.

The entire range of Trelleborg SeaTechnikTM products is also back up by a global service team, ready to support customer operations 24/7. This unrivalled aftersales care means global support with local reach and knowledge.

With over 2,100 exhibitors from 67 countries and 50,000 visitors from 108 nations, SMM gathers representatives across the global shipbuilding and marine equipment industries every two years to discuss the latest innovative technologies in the maritime industry.

To find out more, visit Trelleborg at SSM 2016 on stand 502.

TRELLEBORG TO OPEN 2016 LNG SHIP/SHORE INTERFACE CONFERENCE

By Richard Hepworth, President of Trelleborg’s marine systems operation

Trelleborg’s marine systems operation will deliver the welcoming address at The LNG World Shipping Ship/Shore Interface Conference, which will be held at the Millennium Gloucester Hotel & Conference Centre in London, England, 11-12 May 2016.

Organized by LNG World Shipping, The LNG Ship/Shore Interface Conference provides invaluable best practice insight to all stakeholders in the LNG transportation supply chain. This includes key technology challenges in the LNG transportation sector, such as the ship/shore interface, the growing offshore LNG sector and offshore transfer.

Delivered by Dave Pendleton, Managing Director of Trelleborg’s marine systems operation UK, the welcoming address will discuss the importance of the ship shore interface to LNG transfer. At the conference, Andrew Stafford, Technical Director of Trelleborg’s marine systems operation UK, will also take to the stage to provide an overview of the Ship-Shore Link (SSL) technology that has set the industry standard in large-scale LNG transfer for nearly 20 years. He will also discuss the current compatibility issues in the industry and lessons learned across ship-to-ship transfer, LNGCs and small scale LNG.

With an increasing LNG capacity on stream year-on-year we’re seeing rising demand not only for large scale transportation of cargo, but for more FSRU applications and the growth of LNG fueling for marine vessels. Each of these applications have one key requirement in common: the safe, efficient and timely transfer of LNG from one tank system to another. A critical element in achieving this is the ship shore interface.

The safe, efficient transportation and transfer of LNG as a cargo has had an enviable track record over its 40 year history. The LNG Ship/Shore Interface Conference provides the ideal platform to discuss our commitment to maintaining this record by helping ports, terminals and vessels take a smarter approach to interfaces between units in LNG transfer, which can have a huge impact on overall efficiency.

For more information about The LNG Ship/Shore Interface Conference, or to register your attendance, visit: http://www.lngshippingconference.com

TRELLEBORG TO EXHIBIT AT SEA JAPAN 2016

By Richard Hepworth, President, Trelleborg’s marine systems operation

Trelleborg’s marine systems operation will exhibit its portfolio of advanced marine fender system solutions, docking and mooring equipment, oil and gas transfer technology and surface buoyancy products at Sea Japan 2016, to be held 13 – 15 April at the Tokyo BIG SIGHT Exhibition Center in Tokyo, Japan.

Attracting more than 18,000 high caliber visitors from across the globe, Sea Japan is the country’s largest and fastest growing international commercial marine show.

The Japanese market is very quality-driven, which complements the Trelleborg ethos and our unwavering commitment to taking a smarter approach to port and terminal efficiency.

With that in mind, Sea Japan provides the ideal platform to showcase our comprehensive range of advanced, high performance solutions to one of Trelleborg’s key markets.

On stand, we’ll be showcasing our range of pneumatic and foam fenders. As an ideal ship protection medium for load sensitive structures such as LNG vessels and ocean platforms, Trelleborg’s ISO 17357-1:2014 compliant pneumatic fenders feature high energy absorption with low reaction force. Trelleborg foam fenders are super tough due to a unique manufacturing process and have high energy absorption for their reactive load.

Our booth will also feature our range of IALA compliant, low maintenance, robust navigation buoys. From 1.25 to 3.6m in diameter, these provide a realistic alternative to traditional steel buoys. These modular buoys are lighter, easily transported, lower maintenance and can be deployed using smaller maintenance vessels.

We’ll also be demonstrating its SeaTechnik™ Ship-Shore Link (SSL) system which has been an industry standard in large scale LNG transfer for nearly 20 years and has applications in onshore and offshore applications.

To find out more, visit us at Sea Japan 2016 on booth number N-48. We look forward to meeting you there!

TRELLEBORG SHIPS 600TH LNG SHIP SHORE LINK

By Dave Pendleton, Managing Director, Trelleborg’s marine systems operation, UK

I am delighted to announce that we have recently passed a major milestone with the shipment of our 600th SeaTechnikTM Ship Shore Link (SSL) system for the Liquefied Natural Gas (LNG) Industry.

The SeaTechnikTM SMART SSL system will be installed on a 174,000m3 LNG Carrier (Hull number 2411), being built by Daewoo Shipbuilding & Marine Engineering (DSME) at its Okpo ship yard, Goeje Island, South Korea, for Teekay shipping Limited.

The majority of the world’s LNG cargo fleet and terminals are equipped with SSL technology, a system for communicating the emergency shutdown (ESD) signals, telephone and process data required when cargo transfer is undertaken from ship-to-shore and from shore-to-ship.

We’re proud of our track record in customer service and innovation. Teekay and DSME have been key customers for us since the introduction of the first SeaTechnikTM SSL product 15 years ago. Innovation is an essential part of who we are and we have constantly evolved our technology, from the first analogue systems, to the latest digital systems controlling complex Floating Regasification and Storage Units (FSRU) and LNG fuelling for marine vessels – which include full process data transfer between vessels and terminals.

We view the support service as equally important to the technology itself. A ship costing many tens of thousands of dollars per day to run, and carrying a cargo worth several million dollars, is an expensive asset to have inactive because the SSL interface cannot be connected to transfer the LNG cargo. Our SeatechnikTM SSL technology, and importantly, 24/7 service to test, maintain and repair equipment has a proven track record in making sure this will not happen.

In such an important market, and one that has seen many SSL suppliers come and go, often leaving customers exposed due to lack of support, we are proud of the fact the Trelleborg invested for the long term, and the reward is the 600 SSL milestone.

I’ll leave you with a few words from Odin, Kwon of DSME shipyard and David Glendinning, President of Teekay Gas Services:

Odin said: “As one of the world leaders in the supply of LNG carriers and Floating Regasification and Storage Units (FSRUs), we recognise that the SeaTechnikTM SSL is vital to the performance of our customers’ vessels as a trading asset.”

David said: “Our business is the safe, efficient transport of LNG for our customers. The SSL is a mission critical system in the cargo transfer process. Each of our vessels is also backed by Trelleborg’s Fleet Support Service which ensures an expert is always at the end of the phone or on email, 24/7.”

 

 

 

MARINE SYSTEMS OPERATION SPONSORS PIANC YOUNG PERSONS EVENT

By-line: William Tan, Regional Sales Manager, Trelleborg’s marine systems operation

You may have read that Trelleborg was the official sponsor of PIANC’s latest Young Professionals-Com (YP) networking event, which was held on 27 November at the iconic Boat Quay in Singapore.

YP-Com is dedicated to the career development of PIANC members 40 years of age and younger; locally, nationally and globally. The young persons’ events are designed to encourage global participation within PIANC, and facilitate networking amongst young and senior professionals.

Guests from various fields and regions joined PIANC to share their knowledge and experience, including regional and national consultants, construction companies and suppliers.  With a number of university students also in attendance, the event had a great mix of disciplines and provided a unique opportunity for networking and sharing best practice.

I also took to the stage to discuss a range of key industry issues, as well as Trelleborg’s longstanding association with PIANC.

Feedback was overwhelmingly positive, with many stating what an important platform these events offer for knowledge sharing and deepening learning within the field of marine infrastructure.

I’ll leave you with a couple of words from our Business Unit President to sum up why Trellebrog feels these events are so important.

Richard Hepworth, President of Trelleborg’s marine operation, says: “We have been a PIANC Platinum Partner for over a year now, and feel it’s incredibly important to use this platform to help develop and nurture new talent.  Many of our own employees are part of the PIANC YP program, and we are delighted to continue to be able to share Trelleborg’s research and work with our industry’s new generation.”