Subscribe to RSS

Tag Archives: LNG transfer

TRELLEBORG TO TALK SMARTPORT, TURNKEY LNG SOLUTIONS AT GASTECH 2018

By Richard Hepworth, President of Trelleborg’s marine systems operation


Trelleborg will discuss SmartPort at Gastech in Barcelona (17-20 September), in addition to showcasing its range of game-changing LNG transfer technology. I am also delighted to reveal that as part of Gastech’s main conference program, my colleague Andrew Stafford, Technical Director at Trelleborg’s marine systems operation will present a technical paper discussing the latest in Ship-Shore Link (SSL) technology that has set the industry standard in large-scale LNG transfer for nearly 20 years. Vincent Lagarrigue, Director of Oil & Marine Hoses at Trelleborg’s oil and marine operation will also present a technical paper that outlines how cryogenic floating hose technology is unlocking new possibilities in small to medium-scale transfer and LNG bunkering.

On stand (K160), experts from Trelleborg’s marine systems operation will be on hand to discuss SmartPort, a technology platform that powers the critical interface between ship and port, on land and at sea. The SmartPort platform connects port operations, allowing operators to analyze asset performance and use data to improve decision making. The system integrates assets like fenders, mooring equipment, ship performance monitoring, and navigation systems through a network of sensors.

Trelleborg’s oil and marine operation will be highlighting how their Cryoline floating cryogenic hoses technology is transforming LNG transfer operations in both near-shore and offshore environments. Cryoline technology was specially developed to address pressing infrastructure challenges in the LNG market, enabling turnkey projects that drastically reduce the capex and environmental impact of LNG import infrastructure. It also opens up new locations to ship-to-shore and ship-to-ship transfer, even in challenging weather conditions, and increases safety and operability of FLNG loading and offloading by enabling transfer in tandem configuration.

Trelleborg is able to provide the most integrated and configurable solutions at every interface of the LNG transfer operation. However, realizing the critical interface between ship and port, on land and at sea, SmartPort provides a unique overview of the ‘vessel turnaround’ process, and data extraction points throughout it – both on board the vessel and in the port, and in the interface between the two. We look forward to exhibiting a number of solutions within our SmartPort portfolio including AutoMoor, a rope-free automated mooring system for smarter, safer and more efficient berthing operations; SafePilot, a new generation of piloting and navigation software; as well as our Integrated SSL and Emergency ShutDown System (ESDS) for both large and small-scale LNG transfer and fueling. We’ll also showcase our Quick Release Hooks (QRH) which enable mooring lines to be safely secured and quickly released; as well as its SmartDock Laser Docking Aid System for vessel approach and berthing operations.

In addition to the latest in SSL technology, Andrew’s session will highlight how close co-operation between all parties has enabled Q-LNG to develop their LNG bunkering project from the early adoption for the Harvey Gulf OSV fleet through to the latest requirements for fully flexible bunker vessels. The presentation will also discuss how process safety is improved and training is facilitated by using digital fiber optic link technology with redundancy to ensure compatibility with ESD systems, telephony and cargo process data from any LNG fuelled vessels.

Together, these technologies enable revolutionary new models and thinking for LNG transfer, unlocking new possibilities throughout the transfer zone. Vincent’s session will explore how this was demonstrated in September 2017, when technology from both operations was used in the first sea launch of the Universal Transfer System (UTS), a plug-and-play turnkey developed with Connect LNG. The success of this launch demonstrated the vast potential for new infrastructure possibilities that Trelleborg’s technology enables.

For more information, come and see us on stand K160 at Gastech.

 

TRELLEBORG SUPPLIES SUITE OF SOLUTIONS TO FIRST FLOATING LNG SHIP-TO-SHORE SYSTEM

By Richard Hepworth, President of Trelleborg’s marine systems operation

The recent successful test of the Universal Transfer System (UTS) conducted with Connect LNG and Gas Natural Fenosa is tangible evidence of the new applications that Trelleborg’s suite of products for jettyless LNG transfer can unlock in this challenging field.

The UTS transferred LNG from the Skangas-chartered LNG carrier Coral Energy to the onshore terminal at the Norwegian port of Herøya on October 7 and is now in full commercial operation. A ‘plug and play’ solution, the UTS requires no modifications to the LNG carrier – instead, the platform maneuvers offshore to meet a vessel, removing the need for costly and environmentally intensive dedicated small/medium-scale LNG vessel harbor and jetty structures.

The system consists of Trelleborg’s Cryoline LNG hoses, attached to a floating platform, which incorporates Trelleborg’s ship-shore link technology and a selection of our marine fender systems.

The UTS shows that LNG infrastructure doesn’t need to be bound by the same thinking that underpins transfer solutions for fossil-based energy. Instead, it demonstrates how new ideas are creating the foundations for safe, efficient and convenient infrastructure that can keep pace with the rapid evolution of the LNG market, both as a power source and marine fuel.

The UTS is an important forward thinking development. Our Universal Safety Link (USL) and the Sea Guard and Super Cone fenders are used in many LNG applications already. Integrating them into such an innovative solution as this will help ensure the safe, efficient transfer of LNG into markets and locations that would have previously been considered uneconomic. We are proud to be part of a project that promotes the expansion of the LNG value chain.

The UTS increases the operability of an LNG terminal, as the hose and platform can be retracted when not needed, or when harsh weather conditions would present hazards. The platform-based solution can either function as a standalone unit, or enhance a larger terminal’s ability to handle deliveries to and from a broader range of vessels. Trelleborg service engineers were present during the first commercial LNG transfer of 400m3, and will support further commissioning operations.

A range of Trelleborg technologies make this new model of LNG transfer possible. Cryoline is the first floating hose of its kind to receive the coveted EN1474-2 accreditation, using flexible rubber-bonded hose technology to minimize boil-off and withstand fatigue harsh environmental conditions. Extra safety is provided by an integrated monitoring system using fiber-optic technology.

We also supplied our industry-leading USL 8810 to monitor the LNG transfer process. A triple fiber optic, five pin SIGTTO and pneumatic system was supplied to ensure all round flexibility for the platform for any visiting vessel Our Sea Guard fenders were specified for use at the front of the UTS to absorb berthing impact against the larger LNG vessel prior to attachment to the vessel. While to reduce the impact of the tug vessels on the UTS, our Super Cone (SCN) fenders enable the tugs to safely push the UTS from shore into position for transfer operations.

I’ll leave you with a few comments from Magnus Eikens, Chief Commercial Officer of Connect LNG and José Miguel Moreno, Director at Gas Natural Fenosa:

Magnus commented: “Trelleborg’s expertise in fluid handling and LNG transfer has made it an invaluable partner in this project. The Cryoline LNG hose is an integral part of this solution, thanks to its durability, flexibility, and safety features. What’s more, its ship-shore link technology and marine fender expertise is vital in supporting UTS LNG transfer operations.”

“The innovation demonstrated by Trelleborg and Connect LNG has delivered a game-changing solution for the LNG industry. We now have a market-ready system that opens a world of possibilities in the LNG small and medium scale business thanks to this collaboration,” added Jose.

 

 

 

 

 

TRELLEBORG TO OPEN 2016 LNG SHIP/SHORE INTERFACE CONFERENCE

By Richard Hepworth, President of Trelleborg’s marine systems operation

Trelleborg’s marine systems operation will deliver the welcoming address at The LNG World Shipping Ship/Shore Interface Conference, which will be held at the Millennium Gloucester Hotel & Conference Centre in London, England, 11-12 May 2016.

Organized by LNG World Shipping, The LNG Ship/Shore Interface Conference provides invaluable best practice insight to all stakeholders in the LNG transportation supply chain. This includes key technology challenges in the LNG transportation sector, such as the ship/shore interface, the growing offshore LNG sector and offshore transfer.

Delivered by Dave Pendleton, Managing Director of Trelleborg’s marine systems operation UK, the welcoming address will discuss the importance of the ship shore interface to LNG transfer. At the conference, Andrew Stafford, Technical Director of Trelleborg’s marine systems operation UK, will also take to the stage to provide an overview of the Ship-Shore Link (SSL) technology that has set the industry standard in large-scale LNG transfer for nearly 20 years. He will also discuss the current compatibility issues in the industry and lessons learned across ship-to-ship transfer, LNGCs and small scale LNG.

With an increasing LNG capacity on stream year-on-year we’re seeing rising demand not only for large scale transportation of cargo, but for more FSRU applications and the growth of LNG fueling for marine vessels. Each of these applications have one key requirement in common: the safe, efficient and timely transfer of LNG from one tank system to another. A critical element in achieving this is the ship shore interface.

The safe, efficient transportation and transfer of LNG as a cargo has had an enviable track record over its 40 year history. The LNG Ship/Shore Interface Conference provides the ideal platform to discuss our commitment to maintaining this record by helping ports, terminals and vessels take a smarter approach to interfaces between units in LNG transfer, which can have a huge impact on overall efficiency.

For more information about The LNG Ship/Shore Interface Conference, or to register your attendance, visit: http://www.lngshippingconference.com