Subscribe to RSS

Tag Archives: harbours


The Organisation for Economic Cooperation and Development (OECD)’s International Transport Forum recently released ‘The Impact of Mega Ships’, a new report investigating the impact of larger container ships on infrastructure, equipment and port traffic.

The report, which looks at the pros and cons of the current ‘mega’ container ships, put forward that 24,000 TEU vessels, which could be in service as soon as 2020, will have a major impact on main trade lines, potentially raising transport costs and hindering the competitiveness of ports overall.

We submitted information to the report with regards to the impact that ever increasing vessel sizes are having on port infrastructure, and in particular fenders and docking and mooring equipment such as bollards and hooks.

It’s a timely report. Our latest Barometer Report survey, the fifth that we have conducted, has found that ports are still struggling to keep up with the demands of increasing vessel sizes, especially in terms of onwards logistics.

This is another problem highlighted by the OECD report: although increasing vessel sizes have delivered cost savings in the past, these are decreasing with size, and size-related ‘fixes’ to port and hinterland infrastructure could be substantial.

A more complex challenge

Whilst mega ships bring these increased demands with them, one of the biggest challenges we see is actually designing berths to accommodate the large vessels of the future, whilst ensuring that they are still able to accommodate smaller vessels in the short term.

For our part, this requires fender design that can accommodate a wide range of operating parameters.  Designing a fender system that will perform successfully with kinds of vessel means the rubber compound must be fine-tuned to absorb the required energy, no matter the size of the ship. The properties of the rubber element must be hard enough to withstand the high loads from larger vessels, yet soft enough to accept the loads from smaller vessels.

Bigger ships doesn’t necessarily equal bigger fenders

The new generation of large container vessels uses several fenders at once, which limits the need for increased fender sizes; the extra amount of energy that needs to be absorbed is simply absorbed via more fenders. However, designing for multiple fender contact is still not straightforward for new mega vessels. The considerable bow flare of these ships, designed to accommodate as many containers as possible, mean that even a small berthing angle can lead to contact between the ship and the quay wall equipment.

Taking the pressure off

The rubber component of the fender system can be developed in other ways too, and can even reduce the impact on other port equipment in accommodating mega ships. For example, by designing fender systems with a smaller profile – but more efficient performance characteristics – ports can avoid the often costly process of extending or replacing cranes.

As we see it, ever growing vessel sizes certainly bring with them a whole host of new considerations for ports, not least upgrading infrastructure to allow them to berth. With onwards logistics considerations bringing about their own problems, there needs to be more collaboration and communication across the whole supply chain.

Working with and across suppliers, through an iterative process, from design, is critical to ensuring the port itself benefits from the increased throughput of increased vessel sizes, rather than being hamstrung by it.


Here at Trelleborg, we have provided countless facilities with the customized, high performance solutions needed to optimize their mooring operations. With that in mind, I am delighted to reveal that we have taken the extensive knowledge and expertise gained through our SmartMoor range and applied it to developing a new, streamlined product for customers with less complex requirements, such as those in commercial ports and harbours.

With the ReadyMoor range, a standardized solution that provides the fastest lead times, we now have the ideal solution.

Thanks to its ‘ready-made’ approach, the ReadyMoor range provides a solution that offers the safety and operational benefits of QRHs, whilst passing on commercial benefits to the customer. The series is available with average delivery of just 12 weeks, the time it takes to assemble, test and ship the product.

The compact design of the new range ensures a small installation footprint, minimizing deck space usage and installation costs.

The new hook also reduces maintenance requirements through a single stage locking mechanism, which has fewer moving parts and is available in double or triple hook units with a Safe Working Load (SWL) from 50 tonnes to 150 tonnes. Models with an SWL of 60 tonnes and higher are also available with integral capstans, if required.

To find out more about Trelleborg’s new ReadyMoor range, download the Product Application Briefing now. Alternatively, for a more detailed specification, download the ReadyMoor datasheet at


We are proud to announce the introduction of our rubber quality standards at the world’s largest man-made harbor – The Jebel Ali Port in Dubai. We have been working on the Quay Four refurbishment project with DP world since 2011, and have now completed installation with 60 super cone SCN 1300 fenders to project berths 18 and 19.

Super Cone fenders provide optimal performance and efficiency. The unique design makes them an excellent choice in terms of stability, strength and also resistance to over-compression.

The addition of analytical tests to verify the quality of rubber used in the fenders has ensured us to really reassure the port that the high-performance required for this project will be met.

As the biggest port in the Middle East and a supplier to the global market, we are delighted that DP world has shown commitment to superior solutions by building rubber quality standards in to their fender specifications.

Thanks to our entirely in-house approach, we could even personalise the solution for DP World by including the DP World Logo on the UHMW PE face pads of the fenders.

I will leave you with a few words from Hesham Abdulla, Container Terminal 1 director of DP world, who said: “Trelleborg was able to offer technical support across all parts of the system, from ensuring the rubber element would precisely meet specification, to chains and accessories. Their support and local presence meant that they were a natural choice to supply the project and thanks to their in-house manufacturing capabilities we could even have the solution personalised.”


By Simon Wilson, Managing Director of Docking and Mooring, Trelleborg Marine Systems.

We’ve long stressed the importance of best practice, tailor-made solutions in providing specialist berthing and mooring systems.

It’s important that bespoke, integrated solutions are put in place to enable whole life cost savings and more importantly, ensure safe operations in demanding marine environments.

But, how do you specify a system that optimizes price and value for your particular solution?

Our new bollard guide, written for port operators, and contractors aims to help with just that. The new guide features all the latest comprehensive bollard data, factors to consider in the design process and specification and installation information.

The guide also underlines why different types of bollard are required for different applications and the significance of the differing performance characteristics.

Bollards are safety critical items and as such, product quality is paramount.  The importance of demanding the highest standards of certification is highlighted, with tips on what to look for in a quality documentation package.

To download your free copy of the Bollard Guide, visit


By Richard Hepworth, Managing Director, Trelleborg Marine Systems.

We’ve long considered the need for bespoke solutions and tailored systems to be a key success factor in an efficient and safe port environment. Indeed, we saw further evidence of this when we at Trelleborg won the contract to supply 86 super cone fender systems, 59 mooring bollards with a 200 tonne capacity, and 41 safety ladders for a deep sea container port that handles the largest container ships in the world.

Our solution was chosen after we worked with the port to carry out an in-depth analysis of vessel data and berthing speeds.

Our high-performance Super Cone fenders will be specifically designed for this port to accommodate berthing angles up to 10°, bow flare angles up to 15° and for the latest generation of container vessels with a displacement of 225,000 tons.

The first of the fenders for the container terminal is scheduled for delivery early this year, with the contract scheduled for completion by the end of 2013.

I’ll leave you with some words from one of our area sales managers, Andy Cope, who worked on this project: “We have future-proofed the terminal through the positioning of the fender system.  Therefore, as and when container ship sizes increase, a greater number of fenders will be engaged, absorbing greater levels of impact energy.”

“We have specified the highest quality materials in the design of the fenders, including specialist rubber compounds which have been formulated at our state-of-the-art Singapore facility.  Our in-house capabilities mean that we are able to develop bespoke, yet cost-effective solutions to meet individual project requirements.”


By Simon Wilson, Trelleborg Marine System’s managing director, docking and mooring

Check out our first and second instalments in a series of seven short videos, covering vessel mooring operations from our docking and mooring divisions.

With the latest LNG export terminals requiring modern mooring and monitoring equipment to ensure safe operations, the correct specification of these systems are an essential part of the overall design of marine facilities. The first and second instalments are now live on our YouTube channel.

In the first animation, we introduce the components of a typical system and examine how design can improve safety and reliability in mooring operations. The second instalment covers our field proven Smartdock Docking Aid System and how it assists successful vessel berthing.

Keep an eye out for the next five videos in the series, which will be coming to our YouTube channel over the coming weeks.


By Scott Smith, Regional Director (Asia Pacific), Trelleborg Marine Systems

Indian Centre of Excellence

Trelleborg Marine Systems' newly expanded Indian Centre of Excellence

India West – an online portal for the global Indian community – this week reported that the country’s population still dominates science and engineering with Indian-born US migrants making up the vast majority of graduates in these specialisms (43.1%).

Asia has long been held up for its engineering excellence – with China coming in a close second – so it’s no surprise that global enterprises committed to keeping at the forefront of technical excellence have invested in a strong presence in the region.

Trelleborg has benefitted from a dedicated design and engineering centre in India since 2009 – a resource that is heavily relied upon by the Marine Systems division and other product areas within the Trelleborg Engineered Systems group. Indeed, the centre has become so crucial to our competitive standing as a complete ‘cradle to grave’ supplier that we’ve recently moved to new premises to centralise and expand our unique engineering and design set-up.

While we boast some level of in-house expertise at our regional offices, the more detailed engineering design, modelling and analysis aspects are now sent to the new Indian Centre of Excellence in Ahmedabad, Gujarat, for further progression. Here the business is split into two areas.  The first is engineering and design support for Trelleborg’s worldwide offices – covering Australia, Singapore, China, Japan, India, Dubai, the USA and Europe – and the second focuses on regional sales into India, Pakistan, Sri Lanka and Bangladesh.

We have very high expectations for the performance of the improved engineering and design centre as a market leading offering – not least because, while our competitors choose to outsource their engineering and manufacturing requirements and thereby relinquish some degree of control, having our capabilities centralised in this way means we can maintain watertight quality right through the supply chain. Moreover, it enables us to drive cost efficiencies, improve collaboration and encourage cross fertilisation of ideas across our global offices.

If you’re a port owner, contractor or consultant interested in seeing this unique facility for yourself we’d be happy to give you the guided tour – leave a comment and we’ll get back to you.


By Richard Hepworth, Managing Director, Trelleborg Marine Systems

Salerno Contract Win

The panels for Salerno being prepared. The white marks are a quality control check for the thickness of the paint.

Customers quite rightly demand the ability to meet demanding specifications and tight delivery timescales. Indeed, it’s our capabilities to accommodate stringent design parameters and time pressures that enable me to proudly announce our new contract to supply Super Cone Fenders and Tee Head bollards to Salerno Port, Italy.

Working with RCM Costruzioni, our technical know-how was called upon to overcome restricted space for the cone fender due to a limited high capping beam. What’s more, we also needed to prove that we have the internal processes in place to deliver to exceptionally short lead times with 34 sets of SCN1300 Super Cone Fender Systems and 24 sets of Tee Head bollards 100t required by November. No mean feat!

Fresh from the findings of our latest Barometer report, which brought to the fore that the robust testing of rubber and steel is not routinely performed by all suppliers, I’d like to take this opportunity to point out that all fenders supplied by Trelleborg are fully compliant with PIANC Guidelines and have undergone both laboratory and full scale product testing. Given our industry reputation I’d hope that goes without saying and certainly for our client contact at RCM Construzioni, Mr. Elio Rainone, this played an important part in his decision to specify Trelleborg Marine Systems.

On that note I leave you with some kind words supplied by Mr. Rainone himself and look forward to sharing more company news with you soon…

“Due to Trelleborg’s strong reputation and technical qualification, they are already a preferred supplier for both the port authorities and us, the contractor.

“The solution provided by Trelleborg Marine Systems met the requirements of both parties: the port authorities wanted a reliable solution, with a long life cycle.  For us, an important factor was the necessity of an accessible dedicated project management team, and the assurance of high quality aftercare.”


By Scott Smith, Regional Director (Asia Pacific), Trelleborg Marine Systems

Scott Smith

One of the biggest issues in the market is keeping on top of downtime and maintenance – eight out of 10 ports suffer from unscheduled disruptions with almost half of these being ‘down’ for up to 10 per cent of the time. This was brought to our attention through a recent survey we conducted alongside Lloyds’ List with almost 400 port decision makers.

It revealed that budgets continue to be under pressure and maintenance appears to be suffering because of it. But it’s not all doom and gloom. Things are looking up as new technologies are being harnessed to help overcome issues with port safety and maintenance.

You can download our survey report in full from but if you’re short on time my colleagues and I have put together a series of short videos so you can digest the key findings in more bite-size chunks. Visit the Marine Insights YouTube channel or follow this link to watch at your leisure.


By Richard Hepworth, managing director of Trelleborg Marine Systems

Ports primed for investment surge

It’s immensely pleasing, despite the global downturn, that port owners contractors and consultants are optimistic enough to predict that capital expenditure will rise or at least stay the same over the next 12 months.

At least that was the view of most (55%) decision makers we polled last year as part of a comprehensive market report on the ports, harbours and terminal sector. The Barometer Report, conducted with Port Strategy magazine, also revealed that operational expenditure will remain at current levels or increase with 60% backing this claim.

The apparent optimism is good for the market and good for the economies of the world, which need investment in the global ports to drive trading growth. But I must also sound a note of caution. While the short term outlook is much improved, our research also reveals that these decision makers don’t necessarily expect investment to return to the levels we enjoyed a few years ago. Almost two thirds think it could be less or, at best, static.

The risk of this is only too real. There is a fear that not enough investment will come through to offset the reduction in maintenance we’ve witnessed during the global recession. Ports, harbours and terminals need to embrace the ethos of making adequate investment now to ward off the future costs of downtime.

Trelleborg’s Barometer Report, which details a wide range of findings from the industry survey, is available now as a free download from Takes the Pressure Off.