Subscribe to RSS

Tag Archives: gas

TRELLEBORG SUPPLIES SUITE OF SOLUTIONS TO WORLD’S FIRST FLOATING LNG SHIP-TO-SHORE SYSTEM

By Richard Hepworth, President of Trelleborg’s marine systems operation

The recent successful test of the Universal Transfer System (UTS) conducted with Connect LNG and Gas Natural Fenosa is tangible evidence of the new applications that Trelleborg’s suite of products for jettyless LNG transfer can unlock in this challenging field.

The UTS transferred LNG from the Skangas-chartered LNG carrier Coral Energy to the onshore terminal at the Norwegian port of Herøya on October 7 and is now in full commercial operation. A ‘plug and play’ solution, the UTS requires no modifications to the LNG carrier – instead, the platform maneuvers offshore to meet a vessel, removing the need for costly and environmentally intensive dedicated small/medium-scale LNG vessel harbor and jetty structures.

The system consists of Trelleborg’s Cryoline LNG hoses, attached to a floating platform, which incorporates Trelleborg’s ship-shore link technology and a selection of our marine fender systems.

The UTS shows that LNG infrastructure doesn’t need to be bound by the same thinking that underpins transfer solutions for fossil-based energy. Instead, it demonstrates how new ideas are creating the foundations for safe, efficient and convenient infrastructure that can keep pace with the rapid evolution of the LNG market, both as a power source and marine fuel.

The UTS is an important forward thinking development. Our Universal Safety Link (USL) and the Sea Guard and Super Cone fenders are used in many LNG applications already. Integrating them into such an innovative solution as this will help ensure the safe, efficient transfer of LNG into markets and locations that would have previously been considered uneconomic. We are proud to be part of a project that promotes the expansion of the LNG value chain.

The UTS increases the operability of an LNG terminal, as the hose and platform can be retracted when not needed, or when harsh weather conditions would present hazards. The platform-based solution can either function as a standalone unit, or enhance a larger terminal’s ability to handle deliveries to and from a broader range of vessels. Trelleborg service engineers were present during the first commercial LNG transfer of 400m3, and will support further commissioning operations.

A range of Trelleborg technologies make this new model of LNG transfer possible. Cryoline is the first floating hose of its kind to receive the coveted EN1474-2 accreditation, using flexible rubber-bonded hose technology to minimize boil-off and withstand fatigue harsh environmental conditions. Extra safety is provided by an integrated monitoring system using fiber-optic technology.

We also supplied our industry-leading USL 8810 to monitor the LNG transfer process. A triple fiber optic, five pin SIGTTO and pneumatic system was supplied to ensure all round flexibility for the platform for any visiting vessel Our Sea Guard fenders were specified for use at the front of the UTS to absorb berthing impact against the larger LNG vessel prior to attachment to the vessel. While to reduce the impact of the tug vessels on the UTS, our Super Cone (SCN) fenders enable the tugs to safely push the UTS from shore into position for transfer operations.

I’ll leave you with a few comments from Magnus Eikens, Chief Commercial Officer of Connect LNG and José Miguel Moreno, Director at Gas Natural Fenosa:

Magnus commented: “Trelleborg’s expertise in fluid handling and LNG transfer has made it an invaluable partner in this project. The Cryoline LNG hose is an integral part of this solution, thanks to its durability, flexibility, and safety features. What’s more, its ship-shore link technology and marine fender expertise is vital in supporting UTS LNG transfer operations.”

“The innovation demonstrated by Trelleborg and Connect LNG has delivered a game-changing solution for the LNG industry. We now have a market-ready system that opens a world of possibilities in the LNG small and medium scale business thanks to this collaboration,” added Jose.

 

 

 

 

 

TRELLEBORG SUPPLIES SMARTPORT SOLUTION TO SHELL’S PRELUDE FLNG

By Richard Hepworth, President, Trelleborg’s marine systems operation

I’m delighted to reveal that we have supplied our SafePilot solution, Ship Shore Link (SSL), Electrical Shutdown Link (ESL) and radio ESD for tandem condensate offload to Shell’s Prelude FLNG facility, the largest offshore facility ever constructed. Prelude, which is a staggering 488 meters long, 74 meters wide, and made with more than 260,000 tons of steel, is designed to extract and liquefy natural gas from a site in North West Australia.

We’re proud to have supplied our gas transfer technology and SafePilot navigational and piloting systems to such a large-scale project. The products supplied fall under our SmartPort product range, representing the leading technology we use to enable real time communications and information sharing during vessel approach and transfer operations.

In support of Prelude’s process operations, we supplied our industry-leading SSL system for the transfer of LNG from the platform to visiting LNGCs. In addition, we also provided ESL, known more commonly as the SIGTTO link, for LPG transfer. A new radio ESD link, developed with Shell, was used in conjunction with floating hoses for the tandem transfer of natural gas condensate produced as part of the LNG production process.

We also supplied the navigational system to Prelude, designed to closely monitor the relative motion of the FLNG and the carrier during approach, and the sideways berthing/mooring phase as well as a tandem berthing/mooring phase. The motion and position data of the carrier were measured by the Differential Global Positioning System (DGPS) / Globalnaya Navigazionnaya Sputnikovaya Sistema (GLONASS) RTK based Portable Pilot Units (PPU) which was installed on the bridge wing of the gas LNGC.

The PPU is our “all in one” unit with built in roll and pitch sensors. The CAT III unit is quick and easy to set up, as it only contains two GPS antennas and the PPU switches on automatically the moment the antennas are pulled apart.

The position and motion data of the FLNG is measured by the Motion Reference Unit (MRU) and the DGPS / GLONASS RTK based base station on the FLNG. The base and up to five PPUs were linked via a dedicated UHF frequency.

The offshore operation required our precise approach, monitoring and mooring software for the offshore oil and gas industry. This was done by the SafePilot system, the pilot, master, tug operator and control room all having access to a real-time, accurate and independent picture of the relative positions and movement between the different objects and tankers in operation. Our offshore software allowed the ability to view all objects and shuttle tankers together, on a single display.

For more information on our SmartPort solution, including its SSLs and SafePilot solution, visit: http://ow.ly/qfnA30eKsQo

 

SEE YOU AT KORMARINE 2015!

By Richard Hepworth, President, Trelleborg’s marine systems operation

At the end of October, we will be exhibiting at Kormarine 2015, a leading marine trade exhibition which takes place at the BEXCO (Busan Exhibition & Convention Center), in Busan, Korea and covers international marine, shipbuilding, offshore and oil and gas industries.

At the event, we’re pleased to be demonstrating our new Integrated Ship Shore Link (SSL) and Emergency Shutdown System (ESDS) for the marine LNG industry.

Attracting around 40,000 visitors, Kormarine is the largest marine trade exhibition, covering both commercial and military shipbuilding.

Trelleborg Marine Systems has a major centrer in Busan supporting all of our Oil and Gas Transfer and Vessel Technology products. At the event, representatives from our Busan office, and from the wider business, will be on stand to meet attendees and discuss the latest developments in the Korean market, as well as our experiences in the LNG industry globally.

As well as the new integrated ESDS/SSL system we will also be showcasing our ship performance technology as well as our Worldwide Service capability.

To find out more, visit us at Kormarine 2015 on booth number 5K17, in Hall 5, from the 20 to 23 October. We look forward to meeting you there!

TRELLEBORG ENGINEER JOINS PRESTIGIOUS GASTECH YOUNG ENGINEER FOUNDATION

By Richard Hepworth, President of Trelleborg’s marine systems operation

We call ourselves the Performance People because we ensure the right support is in place for our customers from conceptual design to after sales care. To enable us to deliver truly end-to-end service to our customers, we’re committed to the professional development of our staff.

With that in mind, I am delighted to reveal that Matthew Walker, Project Engineer at our operation in Australia has been handpicked to join the esteemed Gastech Young Engineer Foundation (GYEF).

Given the growing need to attract young talent to the energy industry, the GYEF recognizes and supports the next generation of engineers. The GYEF’s committee, which represents several leading figures in the global energy industry, selected Matthew as one of just 80 successful candidates from several hundred applicants.

Bolstering the professional development of engineers in the early stages of their career, the GYEF has awarded Matthew access to an exclusive package of educational and networking opportunities. This includes a complementary delegate pass for the 2015 Gastech Conference & Exhibition in Singapore (27th – 30th October 2015), providing the opportunity to connect and network with peers and industry leaders. In addition, Matthew has also been awarded a lifetime membership to Gastech’s Young Engineer Alumni and granted unlimited access to online mentoring from thought leaders through a dedicated section of the GYEF website.

For Matthew to be recognized so enthusiastically at such an early stage in his career is a phenomenal feat. We hold a long-standing commitment to the professional development of our staff, and this is testament to our ability to produce industry ready talent.

To find out more about The Gastech Young Engineer Foundation, visit: http://www.youngengineersfoundation.com/

TRELLEBORG BECOMES PIANC PLATINUM PARTNER

Here at Trelleborg, we have a longstanding association with PIANC. Not only do we have a number of people involved in technical working groups, but we’ve also participated in and sponsored a number of world congress events. After being the Platinum AGA sponsor of the 33rd PIANC World Congress at the beginning of June, I am delighted to reveal that we have cemented our commitment to best practice by becoming a PIANC Platinum Partner. As a manufacturer of mission critical port equipment, its essential to us to share knowledge with the industry body that guides standards across the board.

With PIANC continuing to set best practice guidance for so many, and varied, issues pertinent to waterborne transport infrastructure, they felt it was important to have a supplier on board that could contribute across such a broad spectrum.

With our expertise extending from shore-based infrastructure, to oil and gas and LNG; we’re well placed to contribute to a number of areas PIANC work within.

This year’s Congress resolution, set forth by PIANC, will investigate ongoing and emerging trends, technologies and business models. With that said, we here at Trelleborg look forward to being involved in contributing to this important discussion going forward.

For more information about PIANC, visit: www.PIANC.org

SEE YOU AT GASTECH 2014

My colleagues and I will be attending Gastech 2014 in Korea next week. As one of the world’s favorite meeting places for energy professionals working in the oil and gas industry, Gastech provides the ideal platform for us to exhibit our latest product innovations and get some deeper insights into what other delegates see as the most critical issues in the market.

At the show, we’ll be showcasing our brand new Compact Series of Quick Release Hooks (QRHs) which have been designed specifically for smaller and simpler mooring applications, where traditional large and more complex QRHs are not appropriate.

The hooks combine the knowledge of our vastly experienced engineering team with FEA software, and provide an optimized solution for less complex and lower rating mooring applications. They represent a viable alternative to bollards for commercial ports and fuel wharfs, and could also be used in the rapidly developing small-scale LNG sector.

In addition, we’ll also have our Seatechnik™ Universal Safety Link (USL) on stand, a truly innovative product optimized for the small scale LNG sector. The USL was developed in response to the market requirement for a Ship-Shore Link (SSL) which addressed the needs of the LNG marine fuel and small scale transfer market.

We have also developed a new LNG application briefing, ‘Leading-edge Performance in LNG”, which we’ll have available for delegates to take away from our stand. It discusses the evolution of docking and mooring solutions, fender systems and transfer technology across a range of LNG applications.

If you’re heading to Gastech 2014, which will take place at the Kintex, Korea from the 24th to the 27th March, make sure you come and see us on stand F160.

NEW WEBINAR HIGHLIGHTING COMPLEX SYSTEMS INTEGRATION REQUIREMENTS IN FSRUS

Following on from our new whitepaper, “Avoid the Disconnect”, we have also launched a new on-demand webinar for the Liquefied Natural Gas (LNG) sector, which discusses the increasing prevalence of Floating Storage and Regasification Units (FSRUs), the complexity these projects bring about in docking and mooring systems integration, and the importance of considering the jetty, FSRU and LNGC holistically.

The new webinar, “A Comprehensive Approach to FLNG Docking and Mooring Systems”, also examines the differing regulations on design requirements between jetty, FSRU and LNG Carrier, as well as highlighting the importance of centralised monitoring and communications systems, to streamline and align information sharing between all three entities.

In this new webinar, our technical expert will also talk you through the pitfalls of considering docking and mooring systems elements for FSRU projects in isolation and the impact of the mooring system arrangement on systems integration.

To view the new webinar, visit the TrelleborgMarine YouTube channel now: http://ow.ly/pJ8V6