Subscribe to RSS

Tag Archives: Energy

TRELLEBORG SUPPLIES SUITE OF SOLUTIONS TO FIRST FLOATING LNG SHIP-TO-SHORE SYSTEM

By Richard Hepworth, President of Trelleborg’s marine systems operation

The recent successful test of the Universal Transfer System (UTS) conducted with Connect LNG and Gas Natural Fenosa is tangible evidence of the new applications that Trelleborg’s suite of products for jettyless LNG transfer can unlock in this challenging field.

The UTS transferred LNG from the Skangas-chartered LNG carrier Coral Energy to the onshore terminal at the Norwegian port of Herøya on October 7 and is now in full commercial operation. A ‘plug and play’ solution, the UTS requires no modifications to the LNG carrier – instead, the platform maneuvers offshore to meet a vessel, removing the need for costly and environmentally intensive dedicated small/medium-scale LNG vessel harbor and jetty structures.

The system consists of Trelleborg’s Cryoline LNG hoses, attached to a floating platform, which incorporates Trelleborg’s ship-shore link technology and a selection of our marine fender systems.

The UTS shows that LNG infrastructure doesn’t need to be bound by the same thinking that underpins transfer solutions for fossil-based energy. Instead, it demonstrates how new ideas are creating the foundations for safe, efficient and convenient infrastructure that can keep pace with the rapid evolution of the LNG market, both as a power source and marine fuel.

The UTS is an important forward thinking development. Our Universal Safety Link (USL) and the Sea Guard and Super Cone fenders are used in many LNG applications already. Integrating them into such an innovative solution as this will help ensure the safe, efficient transfer of LNG into markets and locations that would have previously been considered uneconomic. We are proud to be part of a project that promotes the expansion of the LNG value chain.

The UTS increases the operability of an LNG terminal, as the hose and platform can be retracted when not needed, or when harsh weather conditions would present hazards. The platform-based solution can either function as a standalone unit, or enhance a larger terminal’s ability to handle deliveries to and from a broader range of vessels. Trelleborg service engineers were present during the first commercial LNG transfer of 400m3, and will support further commissioning operations.

A range of Trelleborg technologies make this new model of LNG transfer possible. Cryoline is the first floating hose of its kind to receive the coveted EN1474-2 accreditation, using flexible rubber-bonded hose technology to minimize boil-off and withstand fatigue harsh environmental conditions. Extra safety is provided by an integrated monitoring system using fiber-optic technology.

We also supplied our industry-leading USL 8810 to monitor the LNG transfer process. A triple fiber optic, five pin SIGTTO and pneumatic system was supplied to ensure all round flexibility for the platform for any visiting vessel Our Sea Guard fenders were specified for use at the front of the UTS to absorb berthing impact against the larger LNG vessel prior to attachment to the vessel. While to reduce the impact of the tug vessels on the UTS, our Super Cone (SCN) fenders enable the tugs to safely push the UTS from shore into position for transfer operations.

I’ll leave you with a few comments from Magnus Eikens, Chief Commercial Officer of Connect LNG and José Miguel Moreno, Director at Gas Natural Fenosa:

Magnus commented: “Trelleborg’s expertise in fluid handling and LNG transfer has made it an invaluable partner in this project. The Cryoline LNG hose is an integral part of this solution, thanks to its durability, flexibility, and safety features. What’s more, its ship-shore link technology and marine fender expertise is vital in supporting UTS LNG transfer operations.”

“The innovation demonstrated by Trelleborg and Connect LNG has delivered a game-changing solution for the LNG industry. We now have a market-ready system that opens a world of possibilities in the LNG small and medium scale business thanks to this collaboration,” added Jose.

 

 

 

 

 

COLLABORATION IS KING FOR THE HALO EFFECT

By Richard Hepworth, President of Trelleborg’s marine systems operation

As part of our recent ‘Preparing for the Port of the Future’ Report, renowned futurist Gerd Leonhard highlighted the need for us an industry to get to grips with the fact that the future isn’t about doing one thing best, it’s about connecting to others that are leading in adjacent and relevant fields.

It’s in this spirit that we’ve forged a new strategic partnership with Teekay Marine Solutions which is part of Teekay, one of the world’s largest marine energy, transportation, storage and production companies.

Bringing together Trelleborg’s manufacturing capability and Teekay’s operations expertise, we’ve launched HALO Fenders, a new premium pneumatic fender offering. With stock in three strategic locations to ensure fast global delivery, there are 32 rental and service bases with a fleet of 400 fenders to ensure we can provide fast, local maintenance and repair.

Working with Teekay, we can provide a premium offering that enables operators to source, deploy and maintain pneumatic fenders safely and efficiently, with a reassuring service structure that ensures these high quality solutions are supported for the life of the project.

We’ve worked closely with Teekay to develop what we believe is an industry leading offer – and one that supports the needs of STS transfer as well as the wider marine market. I believe that HALO Fenders will offer unbeatable safety, reliability and responsiveness – enabling operators to guarantee efficiency and cost-effectiveness.

We’ll be launching HALO Fenders at Gastech in Tokyo (4-7 April), so if you’re attending come and see us on stand 16-320 in hall 2.

 

TRELLEBORG ENGINEER JOINS PRESTIGIOUS GASTECH YOUNG ENGINEER FOUNDATION

By Richard Hepworth, President of Trelleborg’s marine systems operation

We call ourselves the Performance People because we ensure the right support is in place for our customers from conceptual design to after sales care. To enable us to deliver truly end-to-end service to our customers, we’re committed to the professional development of our staff.

With that in mind, I am delighted to reveal that Matthew Walker, Project Engineer at our operation in Australia has been handpicked to join the esteemed Gastech Young Engineer Foundation (GYEF).

Given the growing need to attract young talent to the energy industry, the GYEF recognizes and supports the next generation of engineers. The GYEF’s committee, which represents several leading figures in the global energy industry, selected Matthew as one of just 80 successful candidates from several hundred applicants.

Bolstering the professional development of engineers in the early stages of their career, the GYEF has awarded Matthew access to an exclusive package of educational and networking opportunities. This includes a complementary delegate pass for the 2015 Gastech Conference & Exhibition in Singapore (27th – 30th October 2015), providing the opportunity to connect and network with peers and industry leaders. In addition, Matthew has also been awarded a lifetime membership to Gastech’s Young Engineer Alumni and granted unlimited access to online mentoring from thought leaders through a dedicated section of the GYEF website.

For Matthew to be recognized so enthusiastically at such an early stage in his career is a phenomenal feat. We hold a long-standing commitment to the professional development of our staff, and this is testament to our ability to produce industry ready talent.

To find out more about The Gastech Young Engineer Foundation, visit: http://www.youngengineersfoundation.com/