Subscribe to RSS

Tag Archives: docking

TRELLEBORG MARINE SYSTEMS TO EXHIBIT AT SEA JAPAN 2018

By Richard Hepworth, President, Trelleborg’s marine systems operation

We will be exhibiting our portfolio of advanced marine fender system solutions, docking and mooring equipment, oil and gas transfer technology and piloting solutions at Sea Japan 2018, to be held from 11 to 13 April at the Tokyo Big Sight Exhibition Center in Tokyo, Japan.

Attracting more than 19,000 visitors from across the globe, Sea Japan is the country’s largest and fastest growing international commercial marine show.  Sea Japan provides the ideal platform to showcase our comprehensive range of advanced, high performance solutions to one of Trelleborg’s key markets. Japan, being a highly quality-driven market, complements the Trelleborg ethos and our unwavering commitment to taking a smarter approach to port and terminal efficiency.

On stand, we will showcase SafePilot, our new generation of navigation & piloting software, designed by a dedicated team of software programmers working closely together with worldwide maritime pilots. The result is the most professional and user friendly PPU (Portable Pilot Unit) software. A touch screen interface allows quick interaction to make piloting smoother. The instant zoom function and new intelligent chart structure improves response and decision-making times, giving pilots greater control and accuracy in maneuver.

SafePilot is part of SmartPort, our answer to the need for a standardized way to collect and use data. It’s a technology platform that connects port operations, allowing users to analyze asset performance and apply data insights, to improve day-to-day decision making for optimized operations; improved safety, reduced costs, greater sustainability and increased revenue return. Putting our customers’ needs at the center, SmartPort is setting the true course for consistent commercial success, now and for the future.

To find out more, visit Trelleborg at Sea Japan 2018 on booth number P-48.

TRELLEBORG LAUNCHES AUTOMOOR FOR SMART, ROPE FREE MOORING

By Richard Hepworth, President, Trelleborg’s marine systems operation

Docking and mooring can play a critical role in increasing throughput of an individual berth and overall port facility. No matter the application, ports and terminals worldwide are under pressure to increase throughput. However, trying to do so at the same time as dealing with increasing vessel sizes can be difficult. Optimizing operational windows is an effective route to improving efficiency and one that AutoMoor enables by reducing the time taken to moor vessels.

AutoMoor is a rope-free, automated mooring system that uses smart technologies to enable a faster berthing process and improve safety levels within the port environment. Using vacuum technology to rapidly attach to and secure a vessel at berth, it reduces vessel motions, and continuously monitors all mooring loads acting on the vessel at berth, providing live data to the operator to optimize day-to-day port and terminal operations. It also minimizes personnel involvement to reduce human error and improve safety.

With mooring units that provide real time data to monitor vessel mooring loads, Trelleborg is offering the automated technology needed to compete effectively in today’s complex, global landscape.

Automated mooring technologies minimize downtime by reducing the effects passing ships have on moored vessels. When using mooring lines, operators may need to interrupt operations, costing time and money in delayed product transfer. Using an automated mooring system to dampen vessel motions and extend the range of conditions in which efficient transfer can take place can have huge implications for efficiency.

AutoMoor is also intended to help ports and terminals become more environmentally efficient, because vessels can be secured in under a minute and released in 30 seconds. This reduces vessel idling time and reduces the time tug boats are required alongside the vessel until the mooring operation is complete, cutting emissions overall.

Trelleborg’s AutoMoor solution falls under the operation’s SmartPort portfolio. SmartPort is Trelleborg’s answer to the need for a standardized way to collect and store data in marine applications. It’s a technology platform that connects port operations, allowing users to analyze asset performance and apply data insights, to improve day-to-day decision making.

The most important aspect of SmartPort is the open API structure which enables collaboration with third party systems and third party assets. Historically, Trelleborg has supplied many products for the port environment, from fenders to mooring equipment to ship performance monitoring to navigation and piloting systems: each of which can have their own sensors fitted. By adopting SmartPort architecture, all of these systems and more can be brought under one cloud based system.

To find out more about AutoMoor, download the brochure and discover the smarter approach to docking and mooring: http://ow.ly/ARF330fiAaa

 

CORPORATE AND SOCIAL RESPONSIBILITY FIRMLY ON THE AGENDA AT TRELLEBORG

By Richard Hepworth, President, Trelleborg’s marine systems operation

Testament to the on-going commitment to continuous improvement of the Melbourne manufacturing facility of Trelleborg marine systems operation in Australia, the company’s Environmental Management System (EMS) has been re-certified by Lloyd’s Register Quality Assurance (LRQA) to AS/NZS ISO 14001 environment management standard.

The scope of the EMS certification, which has been maintained to  AS/NZS ISO 14001 since 2010, is applicable to the design, manufacture and commissioning of jetty-based and offshore mooring equipment, monitoring and control systems.

The re-certification of ISO 14001, demonstrates our long-standing commitment to our environmental obligations. Trelleborg’s marine systems operation’s facility in Melbourne, in particular, has made significant strides to advance the environmental impact of its operations in recent years, achieving some truly outstanding results – a huge congratulations to the tireless efforts of those involved.

 

TRELLEBORG TO EXHIBIT AT SEA JAPAN 2016

By Richard Hepworth, President, Trelleborg’s marine systems operation

Trelleborg’s marine systems operation will exhibit its portfolio of advanced marine fender system solutions, docking and mooring equipment, oil and gas transfer technology and surface buoyancy products at Sea Japan 2016, to be held 13 – 15 April at the Tokyo BIG SIGHT Exhibition Center in Tokyo, Japan.

Attracting more than 18,000 high caliber visitors from across the globe, Sea Japan is the country’s largest and fastest growing international commercial marine show.

The Japanese market is very quality-driven, which complements the Trelleborg ethos and our unwavering commitment to taking a smarter approach to port and terminal efficiency.

With that in mind, Sea Japan provides the ideal platform to showcase our comprehensive range of advanced, high performance solutions to one of Trelleborg’s key markets.

On stand, we’ll be showcasing our range of pneumatic and foam fenders. As an ideal ship protection medium for load sensitive structures such as LNG vessels and ocean platforms, Trelleborg’s ISO 17357-1:2014 compliant pneumatic fenders feature high energy absorption with low reaction force. Trelleborg foam fenders are super tough due to a unique manufacturing process and have high energy absorption for their reactive load.

Our booth will also feature our range of IALA compliant, low maintenance, robust navigation buoys. From 1.25 to 3.6m in diameter, these provide a realistic alternative to traditional steel buoys. These modular buoys are lighter, easily transported, lower maintenance and can be deployed using smaller maintenance vessels.

We’ll also be demonstrating its SeaTechnik™ Ship-Shore Link (SSL) system which has been an industry standard in large scale LNG transfer for nearly 20 years and has applications in onshore and offshore applications.

To find out more, visit us at Sea Japan 2016 on booth number N-48. We look forward to meeting you there!

TRELLEBORG COMPLETES ACQUISTION OF MARIMATECH

By Richard Hepworth, President, Trelleborg’s marine systems operation

I am delighted to announce that today, we have signed an agreement to acquire Marimatech A/S, a Danish company that designs and manufactures advanced marine positioning and piloting systems, specializing in the development of software used for docking and mooring ships offshore and in ports. The acquisition is expected to complete in the fourth quarter of this year.

Many of you reading this will already be aware of Marimatech’s portfolio of intelligent docking and mooring solutions, including the SafePilot and other PPUs, Berthing Aid Systems and Environmental Monitoring Systems.

Marimatech’s product portfolio is attractive to us, not only for the obvious synergies with our existing portfolio, but also for the opportunity the integration of both offerings represents.

Marimatech’s navigation and ship positioning product line uses the latest ‘smart’ technology and can be utilized in other applications. This technology can be integrated with our existing range, as we look to take a smarter approach to port and terminal efficiency, and extend the automation that is becoming increasingly well-established on the land side, to the jetty side too.

Of equal importance is the fact that Marimatech truly shares Trelleborg’s standards, having been built on the values of innovation, technology and quality.

Marimatech has a head office and production facility in Aarhus, Denmark, and, like Trelleborg, takes care of the full end to end solution, with in-house design, manufacturing and project management capacity.

I’ve been working closely with Niels Jorgen Vase, Managing Director at Marimatech for the last few months to ensure that the acquisition runs as smoothly as possible, and that both companies continue to deliver the same exceptional levels of service to our customers throughout the transition period. I’m very much looking forward to introducing our two teams and sharing best practice so that our customers can enjoy an enhanced product portfolio and even better service in future.

TRELLEBORG TO HOST SEMINAR IN PARTNERSHIP WITH PIANC

By Richard Hepworth, President of Trelleborg’s marine operation

With PIANC continuing to set best practice guidance for so many, and varied, issues pertinent to waterborne transport infrastructure, we felt that it was only natural to further strengthen our longstanding association.

As such, we will host an exclusive one-day seminar in partnership with PIANC for port consultants. Held on 30th October at the Atlantic Imbizo Conference and Function Studio in Cape Town, South Africa, the free to attend seminar provides us with the ideal opportunity to develop a better understanding of the needs of consultants, so we can evolve our offering to meet them.

The seminar will see Trelleborg experts discuss a range of key industry issues, including the importance of rubber compound composition in the whole-life performance of fender systems and how consultants can determine the formulation of the fenders they procure. This will see our technical expert, Mishra Kumar, discuss mixing and compound modulus as an effective and robust measure of fender performance. The seminar will also provide valuable insight on rubber and foam marine fender design and selection best practice, as well as the latest docking and mooring innovations to improve efficiency and optimize performance.

For more information about the seminar, or if you’d like to register your attendance, contact Anu Bhaskar: anu.bhaskar@trelleborg.com

EXAMINING THE IMPACT OF MEGA SHIPS

The Organisation for Economic Cooperation and Development (OECD)’s International Transport Forum recently released ‘The Impact of Mega Ships’, a new report investigating the impact of larger container ships on infrastructure, equipment and port traffic.

The report, which looks at the pros and cons of the current ‘mega’ container ships, put forward that 24,000 TEU vessels, which could be in service as soon as 2020, will have a major impact on main trade lines, potentially raising transport costs and hindering the competitiveness of ports overall.

We submitted information to the report with regards to the impact that ever increasing vessel sizes are having on port infrastructure, and in particular fenders and docking and mooring equipment such as bollards and hooks.

It’s a timely report. Our latest Barometer Report survey, the fifth that we have conducted, has found that ports are still struggling to keep up with the demands of increasing vessel sizes, especially in terms of onwards logistics.

This is another problem highlighted by the OECD report: although increasing vessel sizes have delivered cost savings in the past, these are decreasing with size, and size-related ‘fixes’ to port and hinterland infrastructure could be substantial.

A more complex challenge

Whilst mega ships bring these increased demands with them, one of the biggest challenges we see is actually designing berths to accommodate the large vessels of the future, whilst ensuring that they are still able to accommodate smaller vessels in the short term.

For our part, this requires fender design that can accommodate a wide range of operating parameters.  Designing a fender system that will perform successfully with kinds of vessel means the rubber compound must be fine-tuned to absorb the required energy, no matter the size of the ship. The properties of the rubber element must be hard enough to withstand the high loads from larger vessels, yet soft enough to accept the loads from smaller vessels.

Bigger ships doesn’t necessarily equal bigger fenders

The new generation of large container vessels uses several fenders at once, which limits the need for increased fender sizes; the extra amount of energy that needs to be absorbed is simply absorbed via more fenders. However, designing for multiple fender contact is still not straightforward for new mega vessels. The considerable bow flare of these ships, designed to accommodate as many containers as possible, mean that even a small berthing angle can lead to contact between the ship and the quay wall equipment.

Taking the pressure off

The rubber component of the fender system can be developed in other ways too, and can even reduce the impact on other port equipment in accommodating mega ships. For example, by designing fender systems with a smaller profile – but more efficient performance characteristics – ports can avoid the often costly process of extending or replacing cranes.

As we see it, ever growing vessel sizes certainly bring with them a whole host of new considerations for ports, not least upgrading infrastructure to allow them to berth. With onwards logistics considerations bringing about their own problems, there needs to be more collaboration and communication across the whole supply chain.

Working with and across suppliers, through an iterative process, from design, is critical to ensuring the port itself benefits from the increased throughput of increased vessel sizes, rather than being hamstrung by it.

LOOKING FORWARD TO THE FLNG WORLD CONGRESS 2015!

Alistair Traylen, Chief Systems Architect, Docking and Mooring Group

At the end of June, I’ll be speaking about developments in the ship-to-ship approach and berthing systems for FLNG at the FLNG World Congress in Singapore.

My presentation will form part of Stream D at the congress, covering ‘Flexible Technology Applications for Cost-Effective FLNG Operations’, and I’ll be discussing technologies, developments and the integration of the ship-to-ship approach and berthing systems, and how they are applicable in the FLNG market.

There are a number of complexities introduced to approach and berthing in ship-to-ship operations, and further arise in the LNG arena. As the FLNG market grows, docking and mooring technology and systems integration need to evolve rapidly to keep up with it.

In particular, I’ll talk about the complexities of banked mooring in terms of berthing and position monitoring, and how they affect the relative positioning requirements for FLNG ship-to-ship berthing. I will also outline considerations for specifying and evaluating ship-to-ship berthing systems.

I’ll leave you with some words from our President, Richard Hepworth, about why this rapidly evolving industry is so important to us, and I hope to see you at the congress!

“Trelleborg is a world leader in the design and manufacture of advanced systems for LNG applications, but we know that we need to continue to innovate to remain in this position.  One of the most valuable ways for us to inform about our developments is through peer-to-peer dialogue, which is just one of the reasons why we feel events like the FLNG World Congress are so important.”

For more information on Trelleborg’s marine systems operation, visit http://www.trelleborg.com/en/Marine-Systems

For more information about the FLNG World Congress, visit: http://www.flngworldcongress.com/

TRELLEBORG TO SHOWCASE NAVIGATION BUOYS AT SEAWORK 2015 INTERNATIONAL

Ashley Tasker, Global Business Development Manager for Marine Products at Trelleborg Marine Systems

I am delighted to reveal that we will showcase our innovative range of IALA compliant modular navigation buoys at Seawork 2015 International, the largest and fastest growing international commercial marine and workboat exhibition and conference held in a European working port environment (16th to 18th June).

Our unique, comprehensive range of navigation buoys provides a solution to fit all demanding requirements – in addition to our standard range, we are able to manufacture to specification where required. The modular system provides an easily transported option to cut down turnaround time and enable fast installation, as they can be shipped in sections and assembled on site.

Manufactured from impact resistant, colour-fast, UV stable materials and comprising of sectional hull pieces filled with marine grade, water-resistant foam, Trelleborg’s range of IALA compliant modular navigation buoys is built around a hot dipped galvanised steel core. Available as standard in diameters ranging from 1.25 to 3.6 meters, Trelleborg will also manufacture precisely to specification where required.

We will also be taking the opportunity to showcase our range of Foam / Elastomer constructed mooring buoys. Thanks to their low maintenance, self-fendering resilient foam bodies and their ease of handling and repair whilst offshore, these are rapidly replacing traditional steel mooring buoys.

Our booth will also feature our pneumatic and foam fenders. As an ideal ship protection medium for load sensitive structures such as LNG vessels and ocean platforms, our range of pneumatic fenders feature high energy absorption with low reaction force. While our foam fenders are super tough due to a unique manufacturing process and have high energy absorption for their reactive load.

If you’re heading to Seawork 2015 and want to find out more, come and see us at booth number A187.

Alternatively, visit: http://www.trelleborg.com/en/Marine-Systems/

TRELLEBORG TO LAUNCH PORT INFRASTRUCTURE AND INNOVATION SEMINAR SERIES

Marco Gaal, Regional Director at Trelleborg’s marine systems operation

Here at Trelleborg, we’re constantly looking for ways to develop our offering to meet new market needs. To do so, we try to ensure that we’re communicating with the market as much as possible to gain valuable insights and feedback on our offering. 

As such, we will be hosting two exclusive one-day seminars featuring the themes of port infrastructure and innovation. Held on 24th March at the Mercure Hotel, Den Haag Leidschendam in Holland, and on 26th March at the Grand Connaught Rooms in London, the free seminars will see myself and a number of colleagues, as well as a number of guest speakers from across the industry, discuss a range of key industry issues, including the optimization of whole-life performance in fender systems. The seminars will provide attendees with valuable insights into marine fender design and selection best practice, and the latest docking and mooring innovations to improve efficiency and improve performance.

The new series of seminars will allow us to talk in-depth with contractors and consultants so we can ensure we’re up to date with the latest market developments and can evolve our offering to meet them.

Ultimately, it’s vital that suppliers meet the needs of their clients by offering support in the areas that customers need it most, be that maintenance, training or other operational requirements across the entire product lifecycle. In our new series of seminars, we’re striving to ensure we do exactly that.

For more information about the conference, or if you’d like to register your attendance at either seminar, visit: http://trelleborg.tecs1.com/Consultant