Subscribe to RSS

Tag Archives: Docking & Mooring

COLLABORATION IS KEY – TRELLEBORG HOSTS THCC SEMINARS

By Richard Hepworth, President, Trelleborg marine systems operation

Vessel sizes are becoming larger, competition is increasing and broader alliances between shipping lines are being established. These factors combine to put increased pressure on ports and terminals. Our industry is famously conservative, but change is coming quickly. There will be a need for more collaboration – as different stakeholders have different strengths. This will make partnerships throughout the supply chain and across industries critical.

After signing a memorandum of understanding (MoU) in 2017, strategically, this is what both we and Third Harbor Consultants Company (THCC) are doing. Collaborating. To further innovation and enable improvements for our ports and vessels. Recently, this saw Trelleborg host two technical seminars (20 & 21 June) in China with consultants and engineers from THCC and CCCC Water Transportation Consultants Company (WTCC).

The seminars provided consultants and engineers from THCC and WTCC with a comprehensive overview of SmartPort by Trelleborg, which powers the critical interface between ship and port, on land and at sea. SmartPort connects port operations, allowing operators to analyze performance and use data to increase efficiencies, improve safety and improve ROI for ports and vessels alike. The system integrates assets like fenders, mooring equipment, ship performance monitoring, and navigation systems through a network of sensors.

The seminars also provided insight on two solutions that fall under the SmartPort portfolio. The first being AutoMoor, Trelleborg’s rope-free, automated mooring system that uses smart technologies to enable faster berthing and improve safety levels within the port environment.

The second was Smart Fender, a marine fender load monitoring system that can be used to measure both the impact on fenders when a vessel berths, and the ongoing force applied as the vessel continues to bear against them whilst docked. When analyzed, the data obtained has the potential to be used in several ways: such as developing a deeper understanding of berthing dynamics, which in turn could assist with future fender and wharf design, and further, feed into the revision of safe and acceptable berthing operations and procedures.

Additionally, load data may be used to determine when maintenance is needed, or indeed, a replacement fender is required. In the event of an accident, or a fender failing, the data can be used to provide information as to why – providing valuable data for insurance claims and helping ports and shipping lines to avoid the costly downtime associated with disputes.

For more on SmartPort by Trelleborg, visit: http://www.trelleborg.com/en/marine-systems/smartport

THE PERFORMANCE PEOPLE LAUNCH NEW STATE-OF-THE-ART WEB PLATFORM

We call ourselves the Performance People because we ensure the right support is in place for our customers from conceptual design to after sales care. With that in mind, we’ve put significant time and effort into redesigning the Trelleborg marine systems operation’s website, to create an easy to navigate web experience for our visitors.

Remaining true to the principles of customer service and product innovation that founded Trelleborg’s marine systems operation over 30 years ago, the new website (which you can view here) provides everything you need to know about each of our six product areas; Marine Fenders, Oil & Gas Transfer, Ship Performance, Docking & Mooring, Surface Buoyancy and Service and Support. Ensuring our resources can be explored more quickly and easily than ever before.

Visitors can access our offering by visiting either the ‘Products, Solutions & Services’ section of the website, if they already know which product they’re looking for. Alternatively, they can search by the  ‘Markets & Applications’ section to see where we could help in their area of interest. The website also has a dedicated ‘Resources’ section, which has everything from product brochures and project requirements forms, through to whitepapers and on-demand webinars.

The new website has been purposefully designed with an emphasis on high quality visuals and graphics showcasing our true capabilities in maintaining and enhancing port and vessel performance. In addition, the new website boasts responsive design technology, which automatically adapts to any viewing device to deliver an optimal, interactive experience wherever you are in the world.

To explore the new website, visit http://www.trelleborg.com/en/Marine-Systems/ and let us know what you think!