Subscribe to RSS

Tag Archives: Big Data

NEW WHITEPAPER PROVIDES OVERVIEW OF BIG DATA IN THE MARITIME SECTOR

By Richard Hepworth, President of Trelleborg’s marine systems operation

Trelleborg’s marine systems operation has launched a new whitepaper bringing together the latest news and thinking on big data in the maritime sector, highlighting how and where these technologies are being implemented and the key application areas that will deliver future operational efficiencies for ports and terminals.

Titled ‘The use of Big Data in the maritime industry’, the whitepaper explores how the maritime industry can better understand the opportunities that big data offers, both now and in the longer term.

Big data has the potential to transform our industry. Through application and insights, big data is creating new opportunities to drive innovation and deliver tangible operational efficiencies across the shipping world.

But the collection of information alone is not enough. It is the analysis of this data and the actionable insights it provides that will transform and increase the efficiency of day-to-day operations across the shipping industry in years to come.

This is a time of huge change for our industry. The advancement of automation, and the exponential rise in data it brings, mean disruption on a scale that ‘shipping’ has never seen before. Those that invest now in the architecture that empowers collaboration between smart assets, will be best equipped to face the future.

SmartPort realises the critical interface between ship and port,
on land and at sea. This gives Trelleborg a unique overview of the ‘vessel turnaround’ process, and data extraction points throughout it – both on board the vessel and in the port, and in the interface between the two. Trelleborg is seeking to educate the marine industry about the importance and potential of this interface.

SmartPort is Trelleborg’s answer to the need for a standardized way to collect and store data. It’s a technology platform that connects port operations, allowing users to analyze asset performance and apply data insights, to improve day-to-day decision making for optimised operations; improved safety, reduced costs, greater sustainability and increased revenue return.

To read the whitepaper, visit: http://ow.ly/ClMF30ihvQc

 

ACTIONS SPEAK LOUDER THAN WORDS

Richard Hepworth of Trelleborg’s marine systems operation considers whether the global shipping industry is keeping up with the technological pace of change.

No-one in the shipping industry denies that automation and Big Data will have a real impact on how we do business, our own research tells us so. But there’s a noticeable disconnect between understanding the significance and opportunities of these new technologies, and actually doing something about them.

According to Trelleborg’s upcoming Preparing for the Port of the Future Report, over 90% of ports, terminals and shippers accept the importance of Big Data, but when it comes to capturing and then interpreting different types of performance data this number drops significantly.

At a time when our industry is under pressure to reduce costs and be more efficient, embracing the opportunity to work smarter should be a priority. There are many different types of data available to port and terminal operators and shipping lines, all of which can deliver real efficiency gains. For example, electronically tracking and standardizing data on pilot performance and adherence to approach routes is monitored by less than a third of operators, yet this has significant impact on areas such as fuel efficiency, missing vessel slots and cost control.

We also know from our research that shipping lines are keen to have greater insights into the speed and angle of berthing but that currently only a fifth of ports offer this. This is just one example of many (see the full Report for more), but it shows that by putting in place smart technologies that enable more sophisticated data capture, there can be benefits for all parties, from improving customer relationships to understanding and avoiding berthing delays.

The old adage of don’t run before you can walk can be applied to Big Data. An easy first step to increase efficiency is to turn existing unstructured data into something useful. Audit, digitize and normalize existing metrics and formats to standardize data. This standardization makes analysis easier to produce informed decision-making that can refine processes, optimize efficiencies, improve safety, identify maintenance and improve customer relationships. And that’s just for starters.

It’s not a case of data becoming the new business currency, it already is. Smart technologies offer an immediate opportunity for port and terminal operators and shipping lines alike, together let’s take advantage of them now.