Subscribe to RSS

Author Archives: hannah.leyland

TRELLEBORG TO PRESENT AT 2019 LNG BUNKERING SUMMIT

By Richard Hepworth, President of Trelleborg’s marine systems operation

Now in its 7th year, the LNG Bunkering Summit focuses on the entire supply chain, offering insights into decision making, planning, development, operation, safety and training processes that are driving the LNG Bunkering market forward. This is Europe’s fastest growing and largest LNG Bunkering Summit at which the future of the industry is discussed annually amongst infrastructure operators, shipping companies, LNG suppliers and technology providers.

With that in mind, I am delighted to reveal that Trelleborg’s marine systems operation will sponsor the 2019 LNG Bunkering Summit, which will be held in Amsterdam, Netherlands (29-31 January).

At the Summit, Paul Radage, Sales Director at Trelleborg’s marine systems operation, will provide a detailed look at a real-life case study in LNG bunkering, discussing the challenges met and the lessons learned.

On stand, Trelleborg will exhibit its Universal Safety Link (USL), an innovative product that takes the company’s expertise in large scale LNG transfer applications, develops it and applies it to provide an optimized product for the burgeoning and diverse small and mid-scale LNG sectors. Delegates will also be able to learn about Trelleborg’s Ship-Shore Link (SSL) technology that has set the industry standard in large-scale LNG transfer for over 20 years.

For more information about Trelleborg’s range of solutions for the LNG industry, visit: http://www.trelleborg.com/en/marine-systems/products–solutions–and–services/ship-shore–links

TRELLEBORG TAKES ITS NAVIGATION AND PILOTING OFFERING TO THE MAX

By Richard Hepworth, President of Trelleborg’s marine systems operation

Trelleborg’s marine systems operation has bolstered its industry leading navigation and piloting offering with the launch of SafePilot CAT MAX, the latest addition to its SafePilot range, which utilizes state-of-the-art software and smart technology to help pilots and ports optimize safety and efficiency in their day-to-day operations.

Replacing its SafePilot CAT III, developed for high positioning accuracy required applications, Trelleborg’s new SafePilot CAT MAX has been specifically designed for use in even more demanding applications including as the piloting of ultra large container vessels and LNG ships in confined waters and offshore operations.

The dual antenna solution, which consists of heading and positioning units which can communicate with each other and the pilot’s display via Wi-Fi, boasts an integrated six-axis gyro/motion sensor, offering precise and independent rate of turn, roll, and pitch. This, coupled with the capability of charging wirelessly, makes the SafePilot CAT MAX the ideal solution for operations where accurate under keel clearance is critical.

Piloting requires the safest, most efficient and reliable technology. It demands exceptional performance, ease of operation and high position accuracy to facilitate optimum approach, berthing and departure. The launch of the SafePilot CAT MAX is the latest example of our long-standing commitment to continually exploring ways in which we can further strengthen our navigation and piloting offering to ensure it delivers exactly that, and then some, in even the most demanding applications.

The SafePilot CAT MAX delivers a speed accuracy down to 1 cm/s and a heading accuracy down to 0.01°, allowing the system to be used in the most challenging operations. Built-in UHF radio facilitates the exchange of environmental, hawser load, product and ESD data between all parts in the operation, including RTK corrections to the CAT MAX. Combined with SafePilot software, this information can also be exchanged via the cloud.

Developed in conjunction with working marine pilots from across the world, SafePilot is known for its intuitive ease of use, offering optional software modules that can be selected according to operational pilotage requirements. Benefits include improved accuracy, as data is filtered to only display what is relevant during each operational phase, eliminating the risk of information overload and enhanced safety through an improved situational overview and accurate, real time data.

SafePilot is a critical component of SmartPort by Trelleborg, which powers the critical interface between ship and port, on land and at sea. It connects port operations, allowing operators to analyze performance and use data to improve decision making. The system integrates assets like fenders, mooring equipment, ship performance monitoring, and navigation systems, underpinned by cloud and Internet of Things (IoT) technologies.

To find out more about SafePilot CAT MAX, visit: https://bit.ly/2C7Uo0T

 

TRELLEBORG STRENGTHENS SAFE PILOTING AND NAVIGATION OFFERING

By Richard Hepworth, President of Trelleborg’s marine systems operation

Trelleborg’s marine systems operation has further bolstered its advanced navigation and piloting offering with the launch of SafeTug, a new software solution that through real-time data sharing, helps tugboat operators and ports to optimize safety and efficiency in their day-to-day operations.

Enhancing collaboration between the tug skipper, bridge team, pilot and port, the SafeTug system uses dynamic data to give tugboat skippers accurate, real-time information on the movement of the ship they are maneuvering. This includes the ship’s speed and direction, rate of turn, trajectory, heading and course over the ground. The software also shows the position of other tugboats using the system.

Piloting requires the safest, most efficient and reliable technology. It demands exceptional performance, ease of operation and high position accuracy to facilitate optimum approach, berthing and departure.

Utilizing the latest technology, SafeTug improves the range and accuracy of navigational measurements, offering true 360° visibility and enhancing situational awareness in real time. This helps the pilot to know exactly where the tugs are located and for the tug master to know exactly what the movement of assisted vessel is, creating a safer and more effective pilotage experience.

SafeTug integrates with SmartPort Cloud, exchanging data to provide an overview of port and piloting operations. It features over-the-air (OTA) differential corrections, real-time traffic overview, live positioning data with predicted paths, data recording, storage and more. Furthermore, the on-shore crew can monitor the whole operation as it happens and by playback for investigation.

Trelleborg’s SafeTug solution falls under the operation’s SmartPort portfolio. SmartPort powers the critical interface between ship and port, on land and at sea. It connects port operations, allowing operators to analyze performance and use data to improve decision making. The system integrates assets like fenders, mooring equipment, ship performance monitoring, and navigation systems, underpinned by cloud and Internet of Things (IoT) technologies.

To find out more about SafeTug, explore Trelleborg’s Situational Awareness experience, visit: https://www.safepilot360experience.com/

 

TRELLEBORG TO KICK-START 2018 LNG SHIP-SHORE INTERFACE CONFERENCE

By Richard Hepworth, President of Trelleborg’s marine systems operation

As Platinum Sponsor, Trelleborg’s marine systems operation will deliver the welcoming address at The LNG Ship/Shore Interface Conference, which will be held in London, UK, 22-23 November 2018.

The LNG Ship/Shore Interface Conference will bring together Europe’s LNG transportation supply chain to discuss ship and terminal operations at the jetty, offshore and bunker station. At the conference, Dave Pendleton, Managing Director of Trelleborg’s marine systems operation in the UK, will deliver the welcoming address and will discuss the importance of businesses investment in innovation, and the critical role that the implementation of innovative solutions plays in the development of global markets. Steve Ward, Technical Sales Manager at Trelleborg’s marine systems operation will also provide a detailed look at a real life case study in LNG bunkering, discussing the challenges met and the lessons learned.

Trelleborg will exhibit its Universal Safety Link (USL), an innovative product that takes the company’s expertise in large scale LNG transfer applications, develops it and applies it to provide an optimized product for the burgeoning and diverse small and mid-scale LNG sectors. Delegates will also be able to learn about Trelleborg’s Ship-Shore Link (SSL) technology that has set the industry standard in large-scale LNG transfer for over 20 years.

Trelleborg will also be exhibiting its USL technology at the Motorship Propulsion and Future Fuels Conference in Hamburg, Germany, 14-16 November 2018. At the conference, which explores the evolution of LNG and other clean, low-flashpoint fuels, Chris Briggs, Technical Sales Engineer at Trelleborg Marine Systems, will take to the stage to discuss the latest in bunkering safety challenges and the importance of compatibility across the industry.

November will also see Trelleborg showcase its Emergency Shutdown Link (ESL) technology for the oil and chemical tanker industry at the 2018 Tanker Shipping & Trade Conference 20 – 21 November) in London, UK, which covers the commercial, operational and technical issues impacting the crude, product and chemical tanker trades.

For more information about Trelleborg’s range of solutions for the LNG industry, visit: http://www.trelleborg.com/en/marine-systems/products–solutions–and–services/ship-shore–links

 

TRELLEBORG JOINS PEMA

By Richard Hepworth, President, Trelleborg’s marine systems operation

Further strengthening our commitment to driving up standards for port and terminal equipment best practice design, manufacturing and testing, I am delighted to reveal that Trelleborg has joined the Port Equipment Manufacturers Association (PEMA).

PEMA represents the interests of those involved in the design, manufacture and supply of port equipment and technology across the globe. Building on our extensive history of collaborative work with industry bodies such as PIANC, Trelleborg has joined PEMA’s ‘Automation & Control Technologies’, ‘Equipment Design & Infrastructure’ and ‘Safety and Environment’ committees which seek to inform, educate and promote best practice, and influence future legislation, policy and standards.

At Trelleborg, disruption has been a key area of focus for us over the last year or so. Our industry is notoriously conservative in embracing new trends and processes, but change is coming, and quickly. This disruption, this radical shaking-up of the shipping, logistics and wider maritime business-model is already underway. We’ve long talked about ‘hyper-collaboration’ – built on the idea that different stakeholders have different strengths – making partnerships throughout the supply chain and across industries not only profitable but necessary to survival.

From Amazon to Maersk and Alibaba, there are many examples of tie-ups and collaborations where non-traditional players, those that understand data and smart technologies, are already transforming our sector. So, for suppliers like ourselves and our fellow PEMA members, it’s about acting now and taking advantage of new technology to provide ports and terminals with new ways to enhance operational efficiency. PEMA provides us with the ideal platform for us to share how both ourselves and others, are doing exactly that.

With the industry facing the challenges of globalization and increasing scale and utilization of vessels, port and terminal equipment suppliers must continuously look for ways to improve efficiencies. Shipping companies and port operators must look for smarter ways to deliver against these expectations. SmartPort by Trelleborg powers the critical interface between ship and port, on land and at sea. Building on Trelleborg’s history of engineering ingenuity and sector knowledge, with a keen eye on data capture and management, and technology-driven insight, SmartPort technologies can increase efficiencies, improve safety and ROI for ports and vessels alike.

SmartPort connects port operations, allowing operators to analyze performance and use data to improve decision making. The system integrates assets like fenders, mooring equipment, ship performance monitoring, and navigation systems, underpinned by cloud and Internet of Things (IoT) technologies.

For more information about SmartPort by Trelleborg, visit: http://www.trelleborg.com/en/marine-systems/smartport

 

TRELLEBORG LAUNCHES NEW FENDER QUALITY FRAMEWORK

By Richard Hepworth, President of Trelleborg’s marine systems operation

Trelleborg’s marine systems operation has launched ‘The Fender Quality Framework’, a new online resource hub designed to help port owners, operators, and specifiers take a smarter approach to fender design and selection.

‘The Fender Quality Framework’ comprises research reports, webinars and more. From design best practice to ingredient selection, manufacturing to performance verification testing, it provides visitors with access to Trelleborg’s near decade of in-depth marine research, which continues to drive up standards for port equipment. The resource will be continuously updated in line with Trelleborg’s marine systems operation’s ongoing efforts to evolve best practice guidance for fender systems.

Ports need to have the confidence that their equipment is fit for purpose to fully protect terminals and berthing vessels, while keeping the port running safely and efficiently. Fenders are an essential part of this port infrastructure and as such their ability to perform reliably day-in, day-out is also essential.

Historically, the industry has undervalued this mission critical equipment, with many often prepared to take a risk on low cost, inferior alternatives. However, decision makers are increasingly giving whole life costs greater precedence, which is naturally steering them towards high quality, high performance fender systems. Trelleborg has long invested significant time and resources to arm specifiers with the information they need to take a smarter approach to fender specification, design and manufacturing. The Fender Quality Framework provides the perfect platform to continue to do exactly that.

To explore The Fender Quality Framework, visit: http://www.fenderqualityframework.com/

 

TRELLEBORG PARTNERS WITH SYNERTEC TO ENHANCE LNG TRANSFER EFFICIENCY ACROSS THE GLOBE

By Richard Hepworth, President of Trelleborg’s marine systems operation

With more LNG capacity coming on stream year on year, we are seeing increasing demand not just for large scale transportation of cargoes but also for more FSRU applications and, of course, the growth of LNG fuelling for marine vessels. All of these applications have one key requirement in common – the safe, efficient and timely transfer of LNG from one tank system to another.

One key critical element in achieving this is the interface between ship and port, on land and at sea – a space that like Trelleborg, leading Australasian engineering consultancy, Synertec specializes within. The ship to shore interface demands that we, across the industry, come together and use all of our skills and talents as technologists and innovators to make it happen, which is exactly what our newly formed strategic partnership with Synertec aims to do.

Under the new agreement, Trelleborg will distribute Synertec’s industry leading LNG custody transfer system across its global sales network. There are clear synergies between the two companies, from our combined technical expertise to our shared commitment to optimizing the interface, which is critical to supporting the business model of every transfer operation. Working with Synertec, we’re able to provide our customers across the globe with an enhanced LNG transfer operation that does exactly that.

LNG custody transfer, the transfer of the ownership of LNG from one organization to other, has long involved fiscal risk given significant uncertainties in traditional tank measurement. Quantities are invoiced in units of transferred LNG based on a calculation of volume, density, and gross caloric value. However, measurement inaccuracies have a significant financial impact for both exporters and importers. For instance, just a one percent error in LNG transferred can result in a significant loss of revenue due to misallocation during custody transfer.

Synertec’s automated custody transfer system, which is ISO 6974, ISO 8943 and GIIGNL (2017) compliant, ensures the precise measurement of loaded LNG, removing the potential for substantial financial losses across the industry and the need for extensive laboratory testing. Used to great success across many high-profile LNG projects across Australasia, the transfer system is a skid mounted module suitable for all LNG applications.

I’ll leave you with some words from Michael Carroll, Managing Director of Synertec: “We’ve built a strong reputation across Australasia and now, boosted by the global reach of Trelleborg, we look forward to meeting the global demand for more accurate and efficient LNG custody transfer.”

For more information about Trelleborg and Synertec’s strategic partnership, visit stand K160 at Gastech (17 – 20 September, 2018).

TRELLEBORG TO TALK SMARTPORT, TURNKEY LNG SOLUTIONS AT GASTECH 2018

By Richard Hepworth, President of Trelleborg’s marine systems operation


Trelleborg will discuss SmartPort at Gastech in Barcelona (17-20 September), in addition to showcasing its range of game-changing LNG transfer technology. I am also delighted to reveal that as part of Gastech’s main conference program, my colleague Andrew Stafford, Technical Director at Trelleborg’s marine systems operation will present a technical paper discussing the latest in Ship-Shore Link (SSL) technology that has set the industry standard in large-scale LNG transfer for nearly 20 years. Vincent Lagarrigue, Director of Oil & Marine Hoses at Trelleborg’s oil and marine operation will also present a technical paper that outlines how cryogenic floating hose technology is unlocking new possibilities in small to medium-scale transfer and LNG bunkering.

On stand (K160), experts from Trelleborg’s marine systems operation will be on hand to discuss SmartPort, a technology platform that powers the critical interface between ship and port, on land and at sea. The SmartPort platform connects port operations, allowing operators to analyze asset performance and use data to improve decision making. The system integrates assets like fenders, mooring equipment, ship performance monitoring, and navigation systems through a network of sensors.

Trelleborg’s oil and marine operation will be highlighting how their Cryoline floating cryogenic hoses technology is transforming LNG transfer operations in both near-shore and offshore environments. Cryoline technology was specially developed to address pressing infrastructure challenges in the LNG market, enabling turnkey projects that drastically reduce the capex and environmental impact of LNG import infrastructure. It also opens up new locations to ship-to-shore and ship-to-ship transfer, even in challenging weather conditions, and increases safety and operability of FLNG loading and offloading by enabling transfer in tandem configuration.

Trelleborg is able to provide the most integrated and configurable solutions at every interface of the LNG transfer operation. However, realizing the critical interface between ship and port, on land and at sea, SmartPort provides a unique overview of the ‘vessel turnaround’ process, and data extraction points throughout it – both on board the vessel and in the port, and in the interface between the two. We look forward to exhibiting a number of solutions within our SmartPort portfolio including AutoMoor, a rope-free automated mooring system for smarter, safer and more efficient berthing operations; SafePilot, a new generation of piloting and navigation software; as well as our Integrated SSL and Emergency ShutDown System (ESDS) for both large and small-scale LNG transfer and fueling. We’ll also showcase our Quick Release Hooks (QRH) which enable mooring lines to be safely secured and quickly released; as well as its SmartDock Laser Docking Aid System for vessel approach and berthing operations.

In addition to the latest in SSL technology, Andrew’s session will highlight how close co-operation between all parties has enabled Q-LNG to develop their LNG bunkering project from the early adoption for the Harvey Gulf OSV fleet through to the latest requirements for fully flexible bunker vessels. The presentation will also discuss how process safety is improved and training is facilitated by using digital fiber optic link technology with redundancy to ensure compatibility with ESD systems, telephony and cargo process data from any LNG fuelled vessels.

Together, these technologies enable revolutionary new models and thinking for LNG transfer, unlocking new possibilities throughout the transfer zone. Vincent’s session will explore how this was demonstrated in September 2017, when technology from both operations was used in the first sea launch of the Universal Transfer System (UTS), a plug-and-play turnkey developed with Connect LNG. The success of this launch demonstrated the vast potential for new infrastructure possibilities that Trelleborg’s technology enables.

For more information, come and see us on stand K160 at Gastech.

 

GUARANTEEING FENDER PERFORMANCE

By Richard Hepworth, President, Trelleborg’s marine systems operation

Trelleborg Fender System

The Thermo-Gravimetric Analysis (TGA) test, adopted by many high quality fender manufacturers, determines whether fenders have been produced using a technically superior rubber formulation that includes little or no recycled rubber and only reinforcing fillers like carbon black.

Reinforcing fillers improve the mechanical properties of rubber. However, contrary to the belief of some across the industry, non-reinforcing fillers such as white calcium carbonate (CaCO3), actually reduces the lifespan of a fender, especially when used in larger quantities. CaCO3 is not a substitute for the carbon black used in high quality fenders.

Considerable research has been carried out over the years on the use of CaCO3 in rubber formulations. It is added to rubber to lower costs, improve processing and impart a lighter color. However, CaCO3 provides very little reinforcement to the rubber. Naturally obtained CaCO3 (ground CaCO3) has poor polymer-filler interaction due to its coarse particle size and its large surface area. Therefore, the rubber compound has poor adhesion and tear resistance.

Some manufacturers make use of large quantities of CaCO3 in the compound formulation of fenders to achieve lower cost. However, while more CaCO3 in a rubber formula may have its advantages in the processing of the compound and lower cost, it negatively impacts the primary aging properties over time, leading to a lower lifespan of the fender.

But, chemical testing is not enough. Full scale testing on prototypes and finished products should also be performed in the manufacturing facility to guarantee that the fenders meet lifecycle and performance specifications. This needs to be verified by testing a randomly chosen fender either at an independent facility, or, by using an independent testing jig.

Although deployed at a manufacturer’s facility using their own test frame, an Independent test rig provides a witness (third party or consultant) with real-time independent testing data captured and shown on an external display. Results are also printed in real-time providing witnesses with direct access to the data. What’s more, load cell and deflection measuring devices can be calibrated on the spot or by an external party independently, outside of the control of the fender manufacturer. Meanwhile test data obtained from the rig can be compared with that reported by manufacturers using their own measuring devices.

It’s vital that the industry understands that the substitution of carbon black with non-reinforcing fillers, such as CaCO3, means that equipment will need to be replaced earlier, and in the long term, result in heavier investment, not to mention the higher risks of failure during service life. Port owners and specifiers also need to educate themselves on the testing methods that can guarantee that the performance of their fenders meet specifications.

For more on Trelleborg’s research into the importance of ingredient selection, mixing and the manufacturing process in marine fenders, please refer to the ‘Guaranteeing Fender Performance’ and ‘Rubber Fenders: Mixing it Up’ whitepapers.

A SMARTER APPROACH TO FOAM FENDERS FOR THE CRUISE INDUSTRY

By Richard Hepworth, President of Trelleborg’s marine systems operation

With cruise ships continuing to grow in size to accommodate the 27.2 million passengers expected to cruise across the globe throughout 2018, it is vital that both terminals and berthing vessels are sufficiently protected. Trelleborg’s marine systems operation has launched a new brochure designed to help port and terminal owners and operators specify industry leading highly versatile foam fenders to meet the needs of the modern cruise terminal.

‘The Smarter Approach: Foam Fenders for the Cruise Industry’ details how Trelleborg’s foam fenders are an easy to use, low maintenance solution that provides many years of reliable service in cruise line operations. Easy to install, they offer a tough, heavy-duty fender solution for in-harbor, off-shore and ship-to-ship applications. Their resilient foam-filled construction provides an unsinkable fender body that permits high energy absorption with relatively low reaction force and hull pressures.

Modern cruise ships are larger than their historic counterparts and so carry more passengers and require a larger crew. In turn, this means more people are dependent on the safety and reliability of the port than ever before. And with the huge capacity of today’s vessels, comes the need for more efficient solutions port side, to accommodate and optimize intended economies of scale.

As a long term supplier and partner to the cruise industry, we’ve gathered our extensive engineering expertise and sector specific knowledge to create the new brochure which provides port and terminal owners and operators with the knowledge they need to achieve faster turnarounds, increased throughput, improve safety and lower operating costs for both their facilities and the vessels that visit them.

Trelleborg’s foam fenders share a construction technology centered on a closed cell polyethylene foam core and an outer skin of reinforced polyurethane elastomer, making punctures a thing of the past. After several years of active service, the fender can be returned to the factory, re-skinned and made ready for a new lease of life. Even if damaged, foam fenders still function until repairs or replacement are possible. To meet the needs of the modern cruise industry, Trelleborg’s foam fenders are available in a range of sizes and performance grades, as well as different colors.

To read the ‘Foam Fenders for the Cruise Industry’ brochure, visit: https://bit.ly/2Jw98Hu